AfuMathOperationSrsToTimeOctave Enumeration¶
NXOpen.CAE.AfuMathOperation.SrsToTimeOctave is an alias for NXOpen.CAE.AfuMathOperationSrsToTimeOctave
-
class
NXOpen.CAE.
AfuMathOperationSrsToTimeOctave
¶ Bases:
object
Defines the octave spacing for SRS to TIME
Enum Members
Enum Member Enum Member Description OneThird 1/3 OctaveOneSixth 1/6 OctaveOneTwelfth 1/12 Octave-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-