ModelDisplayBuilderFreeEdgeFont Enumeration¶
NXOpen.CAE.ModelDisplayBuilder.FreeEdgeFont is an alias for NXOpen.CAE.ModelDisplayBuilderFreeEdgeFont
-
class
NXOpen.CAE.
ModelDisplayBuilderFreeEdgeFont
¶ Bases:
object
specifies the object font for geometry free edges
New in version NX7.5.2.
Enum Members
Enum Member Enum Member Description Solid Solid fontDashed Dashed fontPhantom Phantom fontCenterline Centerline fontDotted Dotted fontLongDashed Long dashed fontDottedDashed Dotted dashed font-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-