LaminateRelabelPliesBuilderRelabelOptionEnum Enumeration

NXOpen.CAE.LaminateRelabelPliesBuilder.RelabelOptionEnum is an alias for NXOpen.CAE.LaminateRelabelPliesBuilderRelabelOptionEnum

class NXOpen.CAE.LaminateRelabelPliesBuilderRelabelOptionEnum

Bases: object

the relabeling option enum.

Enum Members

Enum Member Enum Member Description
LabelAndIncrement
Relabel sequentially using a starting ID and an increment value
Offset
Relabel by applying an offset to existing IDs
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.