BCSelectionDisplayBuilder Class¶
-
class
NXOpen.CAE.
BCSelectionDisplayBuilder
¶ Bases:
NXOpen.Builder
This class provides BC Selection Visual Display support, use this class to get the BC types in current solution, adds special BCs to list, and display the BC’s selection geometry with the BC’s color to do visually check
To create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateBcSelectionDisplayBuilder()
Default values.
Property Value ShowExcludes 0 UseUnspecified 1 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ExcludesColor | Returns or sets the excludes target sets displayed color |
OverlappingColor | Returns or sets the overlapping target sets displayed color |
ShowExcludes | Returns or sets a value indicating how the BCs excluded Model objects will be displayed with the color set by NXOpen.CAE.BCSelectionDisplayBuilder.ExcludesColor() , if True they be displayed using the Excludes Color , if false they be displayed with default color |
Tag | Returns the Tag for this object. |
UnspecifiedColor | Returns or sets the unspecified color for target sets |
UseUnspecified | Returns or sets a value indicating whether the builder will display polygonal geometry or mesh, which do not have these BCs specified on them, with the unspecified color |
Methods¶
Method | Description |
---|---|
AddToSelectedBCsList | Add BCs to the Selected BCs List |
AskBCsByFilter | Return the BCs in the active solution using the specified filters |
AskFamilyNamesByFilter | Returns the list of BC family names used in the current solution. |
AskOverlappingBCs | Returns those BCs which have defined geometries overlapping within the input BCs list |
AskSelectedBCsList | Ask all BCs in the Selected BCs List |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemoveFromSelectedBCsList | Remove BCs from the Selected BCs List |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ExcludesColor¶
-
BCSelectionDisplayBuilder.
ExcludesColor
¶ Returns or sets the excludes target sets displayed color
-------------------------------------
Getter Method
Signature
ExcludesColor()
Returns: Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExcludesColor(excludesColor)
Parameters: excludesColor (Id) – New in version NX10.0.0.
License requirements: None.
OverlappingColor¶
-
BCSelectionDisplayBuilder.
OverlappingColor
¶ Returns or sets the overlapping target sets displayed color
-------------------------------------
Getter Method
Signature
OverlappingColor()
Returns: Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverlappingColor(overlappingColor)
Parameters: overlappingColor (Id) – New in version NX10.0.0.
License requirements: None.
ShowExcludes¶
-
BCSelectionDisplayBuilder.
ShowExcludes
¶ Returns or sets a value indicating how the BCs excluded Model objects will be displayed with the color set by
NXOpen.CAE.BCSelectionDisplayBuilder.ExcludesColor()
, if True they be displayed using the Excludes Color , if false they be displayed with default color-------------------------------------
Getter Method
Signature
ShowExcludes()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowExcludes(showExcludesToggle)
Parameters: showExcludesToggle (bool) – New in version NX10.0.0.
License requirements: None.
UnspecifiedColor¶
-
BCSelectionDisplayBuilder.
UnspecifiedColor
¶ Returns or sets the unspecified color for target sets
-------------------------------------
Getter Method
Signature
UnspecifiedColor()
Returns: Return type: Id New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UnspecifiedColor(unspecifiedColor)
Parameters: unspecifiedColor (Id) – New in version NX10.0.0.
License requirements: None.
UseUnspecified¶
-
BCSelectionDisplayBuilder.
UseUnspecified
¶ Returns or sets a value indicating whether the builder will display polygonal geometry or mesh, which do not have these BCs specified on them, with the unspecified color
-------------------------------------
Getter Method
Signature
UseUnspecified()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseUnspecified(useUnspecifiedToggle)
Parameters: useUnspecifiedToggle (bool) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
AddToSelectedBCsList¶
-
BCSelectionDisplayBuilder.
AddToSelectedBCsList
¶ Add BCs to the Selected BCs List
Signature
AddToSelectedBCsList(bcs)
Parameters: bcs (list of NXOpen.CAE.SimBC
) –New in version NX10.0.0.
License requirements: None.
AskBCsByFilter¶
-
BCSelectionDisplayBuilder.
AskBCsByFilter
¶ Return the BCs in the active solution using the specified filters
Signature
AskBCsByFilter(loadFilter, constraintFilter, simObjFilter, familyFilterNames)
Parameters: - loadFilter (bool) – The load filter status
- constraintFilter (bool) – The constraint filter status
- simObjFilter (bool) – The simulation object filter status
- familyFilterNames (str) – Family filter name, they can be found using
CAE.BCSelectionDisplayBuilder.AskFamilyNamesByFilter()
Returns: Return type: list of
NXOpen.CAE.SimBC
New in version NX10.0.0.
License requirements: None.
AskFamilyNamesByFilter¶
-
BCSelectionDisplayBuilder.
AskFamilyNamesByFilter
¶ Returns the list of BC family names used in the current solution.
Use the returned names as a filter in
BCSelectionDisplayBuilder.AskBCsByFilter()
to get all the BCs with the same family nameSignature
AskFamilyNamesByFilter(loadFilter, constraintFilter, simObjFilter)
Parameters: - loadFilter (bool) – If True, load family names will be included
- constraintFilter (bool) – If True, constraint family names will be included
- simObjFilter (bool) – If True, simulation object family names will be included
Returns: Current family names list, the first filter name will be “All”
Return type: list of str
New in version NX10.0.0.
License requirements: None.
AskOverlappingBCs¶
-
BCSelectionDisplayBuilder.
AskOverlappingBCs
¶ Returns those BCs which have defined geometries overlapping within the input BCs list
Signature
AskOverlappingBCs(bcs)
Parameters: bcs (list of NXOpen.CAE.SimBC
) – CandidateCAE.SimBC
objectsReturns: Overlapping CAE.SimBC
objectsReturn type: list of NXOpen.CAE.SimBC
New in version NX10.0.0.
License requirements: None.
AskSelectedBCsList¶
-
BCSelectionDisplayBuilder.
AskSelectedBCsList
¶ Ask all BCs in the Selected BCs List
Signature
AskSelectedBCsList()
Returns: Return type: list of NXOpen.CAE.SimBC
New in version NX10.0.0.
License requirements: None.
RemoveFromSelectedBCsList¶
-
BCSelectionDisplayBuilder.
RemoveFromSelectedBCsList
¶ Remove BCs from the Selected BCs List
Signature
RemoveFromSelectedBCsList(bcs)
Parameters: bcs (list of NXOpen.CAE.SimBC
) –New in version NX10.0.0.
License requirements: None.
Validate¶
-
BCSelectionDisplayBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.