CAEWeldConnectionBuilderMeshDensityTypeEnum Enumeration

NXOpen.CAE.CAEWeldConnectionBuilder.MeshDensityTypeEnum is an alias for NXOpen.CAE.CAEWeldConnectionBuilderMeshDensityTypeEnum

class NXOpen.CAE.CAEWeldConnectionBuilderMeshDensityTypeEnum

Bases: object

Enum Members

Enum Member Enum Member Description
Size
Size of the each element on the hard object
Number
Number of elements on the hard object
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.