SimGroupContainer Class¶
-
class
NXOpen.CAE.
SimGroupContainer
¶ Bases:
NXOpen.NXObject
Represents UGS::CaeSim::LbcGroupContainer
This is an abstract class
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsConstraintGroupAllowed | Returns a value indicating whether a constraint group is allowed for this group container |
IsLoadGroupAllowed | Returns a value indicating whether a load group is allowed for this group container |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsSimulationObjectGroupAllowed | Returns a value indicating whether a simulation object group is allowed for this group container |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
CreateConstraintGroup | Creates a constraint group for a solution or solution step @return Constraint group CAE.SimConstraintGroup to be created |
CreateLoadGroup | Creates a load group for a solution or solution step @return Load group CAE.SimLoadGroup to be created |
CreateSimulationObjectGroup | Creates a simulation object group for a solution or solution step @return Simulation object group CAE.SimSimulationObjectGroup to be created |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteGroup | Deletes a BC group from this group container |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetGroupCount | Returns the number of groups in this container @return number of groups in the container |
GetGroups | Gets the BC groups in this group container @return the groups in the group container |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsConstraintGroupAllowed¶
-
SimGroupContainer.
IsConstraintGroupAllowed
¶ Returns a value indicating whether a constraint group is allowed for this group container
-------------------------------------
Getter Method
Signature
IsConstraintGroupAllowed()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsLoadGroupAllowed¶
-
SimGroupContainer.
IsLoadGroupAllowed
¶ Returns a value indicating whether a load group is allowed for this group container
-------------------------------------
Getter Method
Signature
IsLoadGroupAllowed()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
SimGroupContainer.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
IsSimulationObjectGroupAllowed¶
-
SimGroupContainer.
IsSimulationObjectGroupAllowed
¶ Returns a value indicating whether a simulation object group is allowed for this group container
-------------------------------------
Getter Method
Signature
IsSimulationObjectGroupAllowed()
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
JournalIdentifier¶
-
SimGroupContainer.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SimGroupContainer.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SimGroupContainer.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SimGroupContainer.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SimGroupContainer.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CreateConstraintGroup¶
-
SimGroupContainer.
CreateConstraintGroup
¶ Creates a constraint group for a solution or solution step
Signature
CreateConstraintGroup()
Returns: Constraint group CAE.SimConstraintGroup
to be createdReturn type: NXOpen.CAE.SimConstraintGroup
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateLoadGroup¶
-
SimGroupContainer.
CreateLoadGroup
¶ Creates a load group for a solution or solution step
Signature
CreateLoadGroup()
Returns: Load group CAE.SimLoadGroup
to be createdReturn type: NXOpen.CAE.SimLoadGroup
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateSimulationObjectGroup¶
-
SimGroupContainer.
CreateSimulationObjectGroup
¶ Creates a simulation object group for a solution or solution step
Signature
CreateSimulationObjectGroup()
Returns: Simulation object group CAE.SimSimulationObjectGroup
to be createdReturn type: NXOpen.CAE.SimSimulationObjectGroup
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteGroup¶
-
SimGroupContainer.
DeleteGroup
¶ Deletes a BC group from this group container
Signature
DeleteGroup(lbGroup)
Parameters: lbGroup ( NXOpen.CAE.SimBcGroup
) – the BC GroupCAE.SimBcGroup
to be deletedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
SimGroupContainer.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetGroupCount¶
-
SimGroupContainer.
GetGroupCount
¶ Returns the number of groups in this container
Signature
GetGroupCount()
Returns: number of groups in the container Return type: int New in version NX4.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetGroups¶
-
SimGroupContainer.
GetGroups
¶ Gets the BC groups in this group container
Signature
GetGroups()
Returns: the groups in the group container Return type: list of NXOpen.CAE.SimBcGroup
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Print¶
-
SimGroupContainer.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SimGroupContainer.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.