BeamEADBuilderEndReleaseSetting Enumeration

NXOpen.CAE.BeamEADBuilder.EndReleaseSetting is an alias for NXOpen.CAE.BeamEADBuilderEndReleaseSetting

class NXOpen.CAE.BeamEADBuilderEndReleaseSetting

Bases: object

indicates which end release setting to use

Enum Members

Enum Member Enum Member Description
Off
end release set to off
On
end release set to on
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.