CorrelShapemetrictype Enumeration¶
-
class
NXOpen.CAE.
CorrelShapemetrictype
¶ Bases:
object
shape Metric Code Enum Members
Enum Member Enum Member Description Mac Shape metric type is Modal Assurance CriteriaComac Shape metric type is Coordinate Modal Assurance CriteriaMsf Shape metric type is Modal Scale FactorsXortho Shape metric type is Cross OrthogonalityNco Shape metric type is Normalized Cross OrthogonalitySco Shape metric type is SEREP-Cross-Orthogonality-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-