PostGraphBuilderDataErrorHandling Enumeration

NXOpen.CAE.PostGraphBuilder.DataErrorHandling is an alias for NXOpen.CAE.PostGraphBuilderDataErrorHandling

class NXOpen.CAE.PostGraphBuilderDataErrorHandling

Bases: object

error handling option when result values are not present for the selected entities

Enum Members

Enum Member Enum Member Description
Skip
UserValue
User given value will used for those entities which do not have result value associated with them
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.