ElementExtrudeBuilderElemDimType Enumeration

NXOpen.CAE.ElementExtrudeBuilder.ElemDimType is an alias for NXOpen.CAE.ElementExtrudeBuilderElemDimType

class NXOpen.CAE.ElementExtrudeBuilderElemDimType

Bases: object

Dimension of element to be created

Enum Members

Enum Member Enum Member Description
Beam
beam
Shell
shell
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.