NodeProjectBuilderProjectionMethodType Enumeration

NXOpen.CAE.NodeProjectBuilder.ProjectionMethodType is an alias for NXOpen.CAE.NodeProjectBuilderProjectionMethodType

class NXOpen.CAE.NodeProjectBuilderProjectionMethodType

Bases: object

Represents Projection Method

Enum Members

Enum Member Enum Member Description
ByDirection
By Direction
ShotestDistance
along shortest distance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.