ASCImporter Class |
Represents a NXOpen.ASCImporter . |
AcisExporter Class |
Represents a AcisExporter to be used when importing the Acis Data This class is created using DexManager . NULL object will be returned from Commit() |
AcisImporter Class |
Represents a AcisImporter to be used when importing the Acis Data This class is created using DexManager . NULL object will be returned from Commit() |
ApparentChainingRule Class |
Represents a NXOpen.SelectionIntentRule that collects curves which appear connected or tangent connected in a particular drafting view. |
Arc Class |
Represents an arc curve. |
ArcCollection Class |
Represents a collection of arcs. |
ArcValidator Class |
validator for curve in a part. |
AssembliesUtils Class |
Contains various assembly utility methods |
AttrTypeKey Class |
This class contains the factory methods for creating a AttrTypeKey. |
AttributeIterator Class |
This class is used to iterate over the user attributes of an object, with options to restrict or extend such searches |
AttributeManager Class |
Provides methods for querying and updating attributes. |
AttributePropertiesBaseBuilder Class |
Represents an NXOpen.AttributePropertiesBaseBuilder to be used for creating attributes. |
AttributePropertiesBuilder Class |
Represents an NXOpen.AttributePropertiesBuilder . |
AttributeTemplatesBuilder Class |
Represents an NXOpen.AttributeTemplatesBuilder to be used when creating attribute templates. |
AutomaticTraceline Class |
Represents an automatic traceline. |
Axis Class |
Represents an NXOpen.Axis class. |
AxisCollection Class |
Represents a collection of NXOpen.Axis . |
BasePart Class |
Base class for an NX part. |
BasePropertyTable Class |
Represents a property table |
BaseSession Class |
Represents a base class for NXOpen session objects. |
BasicEffectivityBuilder Class |
Represent an interface class for basic effectivity block to assign or edit discrete effectivity unit values. |
BcurveValidator Class |
validator for curve in a part. |
Body Class |
Represents a Body |
BodyCollection Class |
Represents a collection of bodies in a part |
BodyDumbRule Class |
Represents a NXOpen.SelectionIntentRule that collects bodies without any intent i. |
BodyFeatureRule Class |
Represents a NXOpen.SelectionIntentRule that collects all bodies created or modified by a feature. |
BodyGroupRule Class |
Represents a NXOpen.SelectionIntentRule that collects all bodies of a group. |
BodyList Class |
Represents a list of objects. |
BodyValidator Class |
validator for a Body in a part. |
Builder Class |
A Builder is an object that is used to create and edit other objects. |
CDF Class |
Represents a NXOpen.CDF , which is a representation of an NX color palette. |
CGMBuilder Class |
Represents a NXOpen.CGMBuilder to be used when exporting the Current Display or drawing sheets to a CGM. |
CGMImporter Class |
Used to import a CGM file into the work part. |
CaeObjectType Class |
Represent options for CAE selection. |
CartesianCoordinateSystem Class |
Represents a cartesian coordinate system |
Catiav4Creator Class |
Represents a NXOpen.Catiav4Creator to be used when exporting the CATIA V4 Data This class is created using NXOpen.DexManager . |
Catiav4Importer Class |
Represents a NXOpen.Catiav4Importer to be used when importing the CATIA V4 Data This class is created using NXOpen.DexManager . |
Catiav5Creator Class |
Represents a NXOpen.Catiav5Creator to be used when exporting the CATIA V5 Data This class is created using NXOpen.DexManager . |
Catiav5Importer Class |
Represents a NXOpen.Catiav5Importer to be used when importing the CATIA V5 Data This class is created using NXOpen.DexManager . |
ClipboardOperationsManager Class |
Used to create importer objects. |
CollaborativeContentManager Class |
Represents the manager for the various collaborative design contents and this class is usable only when NX is running in managed mode. |
CollaborativeDesign Class |
A collaborative design is created in Teamcenter. |
CollaborativeDesignCollection Class |
A collection of collaborative designs. |
ColorDefinition Class |
Represents a NXOpen.ColorDefinition , which is a representation of one color on an NX color palette. |
ColorManager Class |
Contains functionality pertaining to colors |
ColorWidth Class |
Represents a NXOpen.ColorWidth used by NXOpen.WidthDefinition to define a custom width for each color. |
Conic Class |
Represents a conic curve. |
ContentDefinition Class |
Represents a class that defines the contents that will be pulled in to a subset. |
ConvertToFromReferenceBuilder Class |
Represents a NXOpen.ConvertToFromReferenceBuilder |
CoordinateSystem Class |
Represents a coordinate system |
CoordinateSystemCollection Class |
Represents a collection of NXOpen.CoordinateSystem . |
Curve Class |
Represents a curve. |
CurveChainRule Class |
Represents a NXOpen.SelectionIntentRule that collects end-to-end connected curves from the seed curve. |
CurveCollection Class |
Represents a collection of NXOpen.Curve . |
CurveDumbRule Class |
Represents a NXOpen.SelectionIntentRule that collects curves without any intent i. |
CurveFeatureChainRule Class |
Represents a NXOpen.SelectionIntentRule that collects end-to-end connected curves from the feature of the seed. |
CurveFeatureRule Class |
Represents a NXOpen.SelectionIntentRule that collects all curves created by a feature. |
CurveFeatureTangentRule Class |
Represents a NXOpen.SelectionIntentRule that collects tangent connected curves from the feature of the seed. |
CurveGroupRule Class |
Represents a NXOpen.SelectionIntentRule that collects all curves of a group. |
CurveTangentRule Class |
Represents a NXOpen.SelectionIntentRule that collects tangent connected curves from the seed curve. |
CurveValidator Class |
validator for curve in a part. |
CustomPopupMenu Class |
Represents Custom Popup Menu Item class |
CustomPopupMenuHandler Class |
Represents Custom Popup Menu Handler class |
CustomPopupMenuItem Class |
Represents Custom Popup Menu Item class |
CustomWidth Class |
Represents a NXOpen.CustomWidth used by NXOpen.WidthDefinition to define the three custom widths associated with each WidthDefinition. |
CutView Class |
Represents a Cut View |
CutViewCollection Class |
Represents a collection of NXOpen.CutView objects. |
CylindricalCoordinateSystem Class |
Represents a cylindrical coordinate system |
DataContainer Class |
Represents a list of data. |
DateBuilder Class |
The DateBuilder class allows a date and/or time to be input or output via the DateItem builder. |
DateItemBuilder Class |
This class stores a date and time. |
DateItemBuilderList Class |
Represents a list of objects. |
DatumAxis Class |
Represents a datum axis |
DatumCollection Class |
Represents a collection of datum geometry. |
DatumConstraint Class |
Represents a constraint that specifies the location of a NXOpen.Features.DatumFeature . |
DatumPlane Class |
Represents a datum plane |
Decal Class |
Represents a Material Texture decal pair |
DexBuilder Class |
This is an abstract class that provides the basic functionality common to all dex builders. |
DexManager Class |
The DexManager class provides methods to create Dex Builder objects. |
Direction Class |
Represents a direction. |
DirectionCollection Class |
Represents a collection of NXOpen.Direction . |
DisplayManager Class |
Represents an object to manage display settings. |
DisplayModification Class |
Represents changes to the display characteristics of an object. |
DisplayableObject Class |
Base class for all objects that are displayable. |
DraftPointDataCollection Class |
This class contains the factory methods for creating a DraftPointData object. |
DraftingCollectionValidator Class |
validator for DraftingCollection in a part. |
DraftingManager Class |
Represents an object that manages drafting objects and member views. |
DrawingCompareManager Class |
Represents an object that manages drawing compare. |
DrawingUtils Class |
Contains various drawing utility methods |
DxfdwgCreator Class |
Represents a NXOpen.DxfdwgCreator to be used when exporting the DXF/DWG Data This class is created using NXOpen.DexManager . |
DxfdwgImporter Class |
Represents a NXOpen.DxfdwgImporter to be used when importing the DXF/DWG Data This class is created using NXOpen.DexManager . |
Edge Class |
Represents an edge |
EdgeBodyRule Class |
Represents a NXOpen.SelectionIntentRule that collects all the edges of a body. |
EdgeBoundaryRule Class |
Represents a NXOpen.SelectionIntentRule that collects all the edges of a face. |
EdgeChainRule Class |
Represents a NXOpen.SelectionIntentRule that collects end-to-end connected edges from the body of the seed edge. |
EdgeDumbRule Class |
Represents a NXOpen.SelectionIntentRule that collects edges without any intent i. |
EdgeFaceRule Class |
Represents a NXOpen.SelectionIntentRule that collects all edges of a face. |
EdgeFeatureRule Class |
Represents a NXOpen.SelectionIntentRule that collects all edges created or modified by a feature. |
EdgeIntersectRule Class |
Represents a NXOpen.SelectionIntentRule that collects all intersection edges between a set of faces. |
EdgeMultipleSeedTangentRule Class |
Represents a NXOpen.SelectionIntentRule that collects tangent connected edges from the body of the seed edge. |
EdgeSheetBoundaryRule Class |
Represents a NXOpen.SelectionIntentRule that collects boundary edges of a sheet body. |
EdgeTangentRule Class |
Represents a NXOpen.SelectionIntentRule that collects tangent connected edges from the body of the seed edge. |
EdgeValidator Class |
validator for edge in a part. |
EdgeVertexRule Class |
Represents a NXOpen.SelectionIntentRule that collects the vertex edge and and its adjacent edges. |
EdgeVertexTangentRule Class |
Represents a NXOpen.SelectionIntentRule that collects the vertex edge and the edges adjacent and tangent to it. |
EffectivityConditionBuilder Class |
Represent a utility class to assign or edit discrete and range effectivity unit values in the context of a NXOpen.CollaborativeDesign . |
Ellipse Class |
Represents an ellipse curve. |
EllipseCollection Class |
Represents a collection of ellipses. |
EllipseValidator Class |
validator for curve in a part. |
EndCutBlockBuilder Class |
Represents a End Cut Block Builder. |
EngineeringFunction Class |
Contains Engineering Function methods |
ErrorInfo Class |
Contains information about an error that occurred |
ErrorList Class |
Represents a list of errors |
Expression Class |
Represents an expression. |
ExpressionCollection Class |
Represents a collection of expressions. |
ExpressionCollectorSet Class |
An object that binds an expression with an entity section in the context of a list. |
ExpressionCollectorSetList Class |
Represents a list of objects. |
ExpressionGroup Class |
Represents an expression group. |
ExpressionGroupCollection Class |
Represents a collection of expressions groups. |
ExpressionSectionSet Class |
An object that binds an expression with an entity section in the context of a list. |
ExpressionSectionSetList Class |
Represents a list of objects. |
ExpressionValidator Class |
validator for an expression. |
Face Class |
Represents a face |
FaceAdjacentRule Class |
Represents a NXOpen.SelectionIntentRule that collects the faces adjacent to the seed face of a body. |
FaceAllBlendRule Class |
Represents a NXOpen.SelectionIntentRule that collects all blend faces. |
FaceAndAdjacentFacesRule Class |
Represents a NXOpen.SelectionIntentRule that collects both the seed face and all its adjacent faces. |
FaceBodyRule Class |
Represents a NXOpen.SelectionIntentRule that collects all the faces of a body. |
FaceBossPocketFacesRule Class |
Represents a NXOpen.SelectionIntentRule that collects all faces of a boss or pocket. |
FaceConnectedBlendRule Class |
Represents a NXOpen.SelectionIntentRule that collects all connected blend faces. |
FaceDumbRule Class |
Represents a NXOpen.SelectionIntentRule that collects faces without any intent i. |
FaceFeatureRule Class |
Represents a NXOpen.SelectionIntentRule that collects all faces created or modified by a feature. |
FaceMergedRibFacesRule Class |
Represents a NXOpen.SelectionIntentRule that collects all merged rib faces. |
FaceRegionBoundaryRule Class |
Represents a NXOpen.SelectionIntentRule that collects a region of faces that are tangent connected. |
FaceRegionRule Class |
Represents a NXOpen.SelectionIntentRule that collects a region of faces. |
FaceRibFacesRule Class |
Represents a NXOpen.SelectionIntentRule that collects all rib faces. |
FaceSlotFacesRule Class |
Represents a NXOpen.SelectionIntentRule that collects all faces of a pocket. |
FaceTangentRule Class |
Represents a NXOpen.SelectionIntentRule that collects tangent connected faces from the body of the seed face. |
FaceValidator Class |
validator for a Face in a part. |
FeatureCollectionValidator Class |
validator for FeatureCollection in a part. |
FeatureGeneralPropertiesBuilder Class |
Represents a NXOpen.FeatureGeneralPropertiesBuilder to be used for modifying the names of features and general objects. |
FeatureIntersectionEdgesRule Class |
Represents a NXOpen.SelectionIntentRule that collects the intersection edges of boolean like features. |
FeaturePointsRule Class |
Represents a NXOpen.SelectionIntentRule that collects all points created by a feature. |
FeatureProcessBuilderStatus Class |
Represents a NXOpen.FeatureProcessBuilderStatus |
FeatureValidator Class |
validator for a Feature in a part. |
FileNew Class |
Represents a NXOpen.FileNew |
FlatteningBuilder Class |
Represents a FlatteningBuilder builder. It creates a sheet body, as a flattened representation of some other sheet body or faces. |
FollowFilletRule Class |
Represents a NXOpen.SelectionIntentRule that collects curves/edges which are connected or tangent connected and follow onto and off an untrimmed fillet. |
FontCollection Class |
Represents a collection of typographical fonts (for example, Arial, OldEnglish) |
FourPointSurfaceBuilder Class |
Represents a four point sheet body builder |
GeneralScalarTable Class |
Represents a General M x N table of scalar (real) values. |
GenericMeasure Class |
Represents a single valued measurement |
Group Class |
Represents a gateway group |
GroupBuilder Class |
Represents a NXOpen.GroupBuilder |
GroupValidator Class |
validator for a Group in a part. |
HumanData Class |
Represent the data used to create the human |
HumanHandShapeData Class |
Represent hand shape data |
HumanPosturePrediction Class |
Represent posture prediction object |
HumanPosturePredictionBuilder Class |
Represents a Human Posture Prediction Builder. |
HumanReachZone Class |
Represents a human reach zone. |
Hyperbola Class |
Represents a hyperbola curve. |
HyperbolaCollection Class |
Represents a collection of hyperbolas. |
HyperbolaValidator Class |
validator for curve in a part. |
IAttributeSourceObjectBuilder Class |
Represents an interface to perform various database operations on an array of NXOpen.NXObject . |
IBaseCurve Class |
Represents something containing a two dimensional curve |
IBasePlane Class |
Represents a Plane or Datum Plane |
IBody Class |
Represents something containing a body |
ICurve Class |
Represents something containing a two dimensional modeling curve |
IFitTo Class |
Represents something that can be supplied to View.FitToObjects() |
ILocation Class |
Represents something that can be supplied to an location selection |
INXObject Class |
Represents an interface from which most NXOpen classes inherit |
IOrientation Class |
Represents something that can be supplied to an orientation selection |
IParameterizedSurface Class |
Represents something containing a face |
IPlane Class |
Represents an Plane class. |
IProfile Class |
Represents something that can be supplied to a profile |
IReferenceAxis Class |
Represents an object that could be used as a reference axis for a feature |
ISketchHelpedConstraint Class |
Represents a sketch constraint that has a help point or help parameter. |
ISurface Class |
Represents something containing a two dimensional surface |
ITableEditorDataProvider Class |
Interface for providing basic data for a Table Editor block. |
IgesCreator Class |
Represents a NXOpen.IgesCreator to be used when exporting the IGES Data This class is created using NXOpen.DexManager . |
IgesImporter Class |
Represents a NXOpen.IgesImporter to be used when importing the IGES Data This class is created using NXOpen.DexManager . |
ImportManager Class |
Used to create importer objects. |
Importer Class |
Base class for importing data into the work part. |
InferSnapType Class |
Represent options for snap selection. |
InferredConstraintsBuilder Class |
Represents a NXOpen.InferredConstraintsBuilder |
InfiniteLine Class |
Represents a infinite line curve. |
InfiniteLineCollection Class |
Represents a collection of infinite lines. |
Information Class |
Represents a class that provides methods for displaying information about part history, interpart parents and children, features, points, and other NX Objects. |
InterpartExpressionsBuilder Class |
This class creates interpart expressions from the source part to the current work part via the naming rule defined. |
JamSession Class |
Represents a Jam session |
JournalManager Class |
Represents the JournalManager which is used to query data about journals when recording and replaying journal files. |
JtCreator Class |
Represents a NXOpen.JtCreator to be used when exporting the JT Data This class is created using NXOpen.PvtransManager . |
KFObject Class |
Represents an KF object in the part. |
Layout Class |
Represents a layout. |
LayoutCollection Class |
Represents a collection of layouts. |
LayoutDefinition Class |
Represents the definition of a layout. |
LicenseManager Class |
Provides utility methods for managing licenses. |
Light Class |
Represents a light source. |
LightCollection Class |
Represents a collection of :py:class:`NXOpen.Light`s. |
Line Class |
Represents a line curve. |
LineCollection Class |
Represents a collection of lines. |
LineColorFontWidthBuilder Class |
Represent a NXOpen.LineColorFontWidthBuilder |
LineFontBuilder Class |
Represent a NXOpen.LineFontBuilder |
LineValidator Class |
validator for curve in a part. |
LineWidthBuilder Class |
Represents a NXOpen.LineWidthBuilder |
LinkedMirrorPartAttributeEditData Class |
JA interface for LinkedMirrorPartAttributeEditData object |
LinkedMirrorPartAttributeEditEvent Class |
JA interface for LinkedMirrorPartAttributeEditEvent object |
LinkedMirrorPartBuilder Class |
builder class of LinkedMirrorPartBuilder |
LinkedMirrorPartEntityMapData Class |
JA interface for LinkedMirrorPartEntityMapData oject |
LinkedMirrorPartEntityMapEvent Class |
JA interface for LinkedMirrorPartEntityMapEvent object |
LinkedPartManager Class |
Represents the customization interface during linked mirror part creation and update. |
ListCreator Class |
Represents a NXOpen.ListCreator to be used when exporting the JT Data This class is created using NXOpen.PvtransManager . |
ListCreatorList Class |
Represents a list of objects. |
ListingWindow Class |
Represents a ListingWindow. |
LoadOptions Class |
Contains accessor methods for all the part load options. |
LogFile Class |
Represents the system log file |
MWUpdate Class |
Update tools used in Mold Wizard for the Journamation layer |
MassPropertiesBuilder Class |
Represents a NXOpen.MassPropertiesBuilder for calculating the weight of selected objects as well as informing the part that the assemblies weight property data needs to be updated on save. |
Material Class |
Represents Material |
MaterialManager Class |
A manager to deal with all material objects |
MaterialUtilities Class |
Represents Physical NXOpen.MaterialUtilities class |
MathUtils Class |
Contains various math utility methods |
Measure Class |
Represents a measurement feature |
MeasureAngle Class |
Represents a single valued Angle measurement |
MeasureAngleBuilder Class |
Represents a NXOpen.MeasureAngleBuilder |
MeasureBodies Class |
Represents the measurement specific mass properties for a set of bodies |
MeasureBodyBuilder Class |
Represents a NXOpen.MeasureBodyBuilder |
MeasureBuilder Class |
Represents a NXOpen.MeasureBuilder |
MeasureDistance Class |
Represents a single valued distance measurement |
MeasureDistanceBuilder Class |
Represents a NXOpen.MeasureDistanceBuilder |
MeasureFaceBuilder Class |
Represents a NXOpen.MeasureFaceBuilder |
MeasureFaces Class |
Represents the measurement of perimeter and area of a set of faces |
MeasureLength Class |
Represents a single valued length measurement |
MeasureManager Class |
Provides methods for manipulating the measurement objects in a part. |
MeasurePoint Class |
Represents a point measurement |
MeasurePolarAngle Class |
Represents a single valued polar angle measurement |
MeasurePolarArea Class |
Represents a single valued polar area measurement |
MeasurePolarRadius Class |
Represents a single valued polar radius measurement |
MeasureRectangularExtreme Class |
Represents a rectangular extreme point measurement |
Measurement Class |
Provides methods for calculating and displaying the measurement information. |
MechatronicsBaseValidator Class |
validator for a mechatronics feature in a part. |
MechatronicsDebugSession Class |
Represents a class that is used for NX MECHATRONICS Autotest. |
MeshParameterData Class |
Represents surface rebuild data structure. |
MeshProfileString Class |
Represents Mesh profile string |
ModelingView Class |
Represents a Modeling View |
ModelingViewCollection Class |
Represents a collection of :py:class:`ModelingView`s. |
ModelingViewHighQualityImage Class |
Represents the properties and methods for generating a High Quality Imageof a Modeling View |
MovieManager Class |
Represents a MovieManager class. This class is used for recording movies. |
MovieSettingsBuilder Class |
This class is the builder for the Movie Settings. |
NXColor Class |
Represents a standard NX color. |
NXMatrix Class |
Represents an NX matrix. |
NXMatrixCollection Class |
Represents a collection of NX Matrixes. |
NXMessageBox Class |
Displays message box. |
NXObject Class |
A base class providing low-level services for most NXOpen classes. |
NXObjectList Class |
Represents a list of objects. |
NXTo2dCreator Class |
Represents a NXOpen.NXTo2dCreator to be used when exporting the 2D Data This class is created using NXOpen.DexManager . |
NavigatorFilter Class |
Represents a NXOpen.NavigatorFilter object. |
NonFeatureSmartContainer Class |
Represents a Non Feature Smart Container |
OMAttribute Class |
Represents a OMAttribute. |
OMClass Class |
Represents a OMClass. |
OMSchema Class |
Represents a OMSchema. |
ObjectGeneralPropertiesBuilder Class |
Represents an NXOpen.ObjectGeneralPropertiesBuilder to be used for modifying the names and properties of objects. |
ObjectList Class |
Represents a list of objects. |
ObjectSelector Class |
Represents a NXOpen.ObjectSelector to be used when exporting the the selected objects from NX part. |
ObjectTypeSelector Class |
Represents a NXOpen.ObjectTypeSelector to be used when filter out the objects based on the type during import/export. |
Offset Class |
Represents a NXOpen.Offset . |
OffsetCollection Class |
Represents a collection of NXOpen.Offset . |
OuterEdgesOfFacesRule Class |
Represents a NXOpen.SelectionIntentRule that collects the outer edges of a group of faces. |
Parabola Class |
Represents a parabola curve. |
ParabolaCollection Class |
Represents a collection of Parabolas |
ParabolaValidator Class |
validator for curve in a part. |
Part Class |
Represents an NX part of type .prt. |
PartCleanup Class |
Provides utilities to to eliminate certain inaccessibleobjects from the part file. |
PartCloseResponses Class |
Manages a list of part name/response pairs which areused to determine whether a part should be closed if modified duringpart close. |
PartCloseStatus Class |
This class represents a list of part names with associated status codes that serve to communicate why these parts were not able to be closed. |
PartCollection Class |
Represents the collection of all parts in a session. |
PartDelayedUpdateStatus Class |
Represents a list of part names with associated delay status codes. |
PartFamilyManager Class |
This class represents part family |
PartFamilyMemberData Class |
This class is responsible for storing part family member data Use the method NXOpen.Part.NewPartFamilyMemberData() to create new instance of this class. |
PartFamilyMemberValues Class |
This class is responsible for storing part family member attribute values. |
PartImporter Class |
Used to import a part into the work part. |
PartLoadStatus Class |
Represents a list of part names with associated status codes. |
PartNavigatorValidator Class |
validator for partnavigator in a part. |
PartReopenReport Class |
Contains information about a part and its components after it has beenreopened. |
PartReopenStatus Class |
Contains information about a part after an attempt was made toreopen it. |
PartSaveOptions Class |
Contains accessor methods for all part save options that follow the part. |
PartSaveStatus Class |
This class represents a list of part names with associated status codes that serve to communicate why these parts where not able to be saved during part save. |
PasteSpecialBuilder Class |
Represents a NXOpen.PasteSpecialBuilder |
PerformanceManager Class |
Represents class containing APIs used for monitoring performance. |
PhysicalMaterial Class |
Represents Physical Material |
PhysicalMaterialBuilder Class |
Represents a NXOpen.PhysicalMaterial builder |
PhysicalMaterialCollection Class |
Represents the collection of all NXOpen.PhysicalMaterial objects in this Part |
Plane Class |
Represents an Plane class. |
PlaneCollection Class |
Represents a collection of NXOpen.Plane . |
PlaneList Class |
Represents a list of objects. |
PlaneTypes Class |
Represents an NXOpen.PlaneTypes class. |
PlmObjectNode Class |
This class contains the factory methods for creating a PlmObjectNode. |
PlotBuilder Class |
Represents a NXOpen.PlotBuilder . |
PlotColorsWidthsBuilder Class |
Represents a NXOpen.PlotColorsWidthsBuilder to be used for plotting. |
PlotManager Class |
The PlotManager class provides methods to create Gateway Builder objects. |
PlotSourceBuilder Class |
Represents a NXOpen.PlotSourceBuilder All sheets provided must be in the displayed part. |
Point Class |
Represents a smart Point . |
PointCollection Class |
Represents a collection of smart NXOpen.Point . |
PointList Class |
Represents a list of objects. |
PointValidator Class |
validator for curve in a part. |
Polyline Class |
Represents a polyline curve. |
PolylineCollection Class |
Represents a collection of polylines. |
PositioningDimension Class |
Represents a dimension object attached to the feature |
PreviewPropertiesBuilder Class |
Represents a NXOpen.PreviewPropertiesBuilder to be used for creating and storing previews. |
Print3dBuilder Class |
This class sends the 3d model for 3dprinting. |
PrintBuilder Class |
Represents a NXOpen.PrintBuilder . |
PrintPDFBuilder Class |
Represents a NXOpen.PrintPDFBuilder to be used when exporting the Current Display or selected sheets to a PDF document. |
ProeImporter Class |
Represents a NXOpen.ProeImporter to be used when importing the ProE Data This class is created using NXOpen.DexManager . |
PropertiesManager Class |
The PropertiesManager class provides methods to create Gateway Properties Builder objects. |
PropertyContainer Class |
Represents a list of properties. |
PvtransManager Class |
The PvtransManager class provides methods to create Pvtrans Builder objects. |
ReferenceSet Class |
Represents a NXOpen.ReferenceSet . |
RegionBoundaryRule Class |
Represents a NXOpen.SelectionIntentRule that collects curves as specified by an enclosed region. |
RegionPoint Class |
Represents a point and body context on a region point. |
RegionPointList Class |
Represents a list of objects. |
RemoteUtilities Class |
This class is primarily designed for use in a remote session, and allows client applications to access resources on a remote server. |
ReplaceExpressionsBuilder Class |
This class creates Replace expressions from the source part to the current work part via the naming rule defined. |
RibTopFaceEdgesRule Class |
Represents a NXOpen.SelectionIntentRule that collects the like convexity outer edges of a group of faces. |
RuleManager Class |
Provides methods for manipulating the Knowledge Fusion rules in a part. |
STLImporter Class |
Used to import an STL file into the work part. |
SaveOptions Class |
Contains accessor methods for all part save options that follow the session. |
ScCollector Class |
Sc Collector |
ScCollectorCollection Class |
This class contains the factory methods for creating a sc collector. |
ScCollectorList Class |
Represents a list of objects. |
ScRuleFactory Class |
This class contains the factory methods for creating selection intent rules |
Scalar Class |
Represents a scalar. |
ScalarCollection Class |
Represents a collection of NXOpen.Scalar objects. |
ScalarMatrixValue Class |
Represents a General M x N matrix of scalar (real) values. |
ScalarTableValue Class |
Represents a General M x N table of scalar (real) values. |
Section Class |
Represents a section |
SectionCollection Class |
This class contains the factory methods for creating a section. |
SectionData Class |
Represents section data |
SectionElementData Class |
Represents section element data |
SectionList Class |
Represents a list of objects. |
SelectBody Class |
Represents a single object selection. |
SelectBodyList Class |
Represents a list of objects on a selection list. |
SelectCartesianCoordinateSystem Class |
Represents a single object selection. |
SelectCoordinateSystem Class |
Represents a single object selection. |
SelectCoordinateSystemList Class |
Represents a list of objects on a selection list. |
SelectCurve Class |
Represents a single object selection. |
SelectCurveList Class |
Represents a list of objects on a selection list. |
SelectDatumPlane Class |
Represents a single object selection. |
SelectDatumPlaneList Class |
Represents a list of objects on a selection list. |
SelectDisplayableObject Class |
Represents a single object selection. |
SelectDisplayableObjectList Class |
Represents a list of objects on a selection list. |
SelectEdge Class |
Represents a single object selection. |
SelectEdgeList Class |
Represents a list of objects on a selection list. |
SelectExpressionList Class |
Represents a list of objects on a selection list. |
SelectFace Class |
Represents a single object selection. |
SelectFaceList Class |
Represents a list of objects on a selection list. |
SelectGroup Class |
Represents a single object selection. |
SelectIBaseCurve Class |
Represents a single object selection. |
SelectIBaseCurveList Class |
Represents a list of objects on a selection list. |
SelectIBasePlaneList Class |
Represents a list of objects on a selection list. |
SelectICurve Class |
Represents a single object selection. |
SelectICurveList Class |
Represents a list of objects on a selection list. |
SelectINXObjectList Class |
Represents a list of objects on a selection list. |
SelectIParameterizedSurface Class |
Represents a single object selection. |
SelectIParameterizedSurfaceList Class |
Represents a list of objects on a selection list. |
SelectIReferenceAxis Class |
Represents a single object selection. |
SelectISurface Class |
Represents a single object selection. |
SelectLine Class |
Represents a single object selection. |
SelectNXObject Class |
Represents a single object selection. |
SelectNXObjectList Class |
Represents a list of objects on a selection list. |
SelectObject Class |
Represents a single object selection. |
SelectObjectList Class |
Represents a list of objects on a selection list. |
SelectPart Class |
Represents a single object selection. |
SelectPartList Class |
Represents a list of objects on a selection list. |
SelectPoint Class |
Represents a single object selection. |
SelectPointList Class |
Represents a list of objects on a selection list. |
SelectSketch Class |
Represents a single object selection. |
SelectSmartObject Class |
Represents a single object selection. |
SelectSpline Class |
Represents a single object selection. |
SelectSplineList Class |
Represents a list of objects on a selection list. |
SelectTaggedObject Class |
Represents a single object selection. |
SelectTaggedObjectList Class |
Represents a list of objects on a selection list. |
SelectView Class |
Represents a single object selection. |
Selection Class |
Defines an interface object for executing selection operations |
SelectionHandle Class |
Represents a SelectionHandle for UI Styler |
SelectionIntentRule Class |
Represents a NXOpen.SelectionIntentRule which essentially provides capabilities to collect curves, edges, faces and bodies. |
SelectionMethod Class |
Represents the output from a smart selector method |
SelectionSubscriber Class |
Defines a SelectionSubscriber for managing selection events |
Session Class |
Represents the NX session. |
ShipBaseDrawingValidator Class |
validator for a ship drawing in a part. |
ShipBaseValidator Class |
validator for a ship feature in a part. |
SingleMeasure Class |
Represents a single valued measurement |
Sketch Class |
Represents a sketch |
SketchAlignmentConstraint Class |
Represents a sketch alignment constraint |
SketchAlongPathBuilder Class |
Use the NXOpen.SketchAlongPathBuilder to create or reattach a NXOpen.Sketch along a path. |
SketchAngularDimensionBuilder Class |
Represents a NXOpen.SketchAngularDimensionBuilder |
SketchAssociativeTrim Class |
Represents a sketch associative trim constraint |
SketchAssociativeTrimBuilder Class |
Represents a NXOpen.SketchAssociativeTrimBuilder |
SketchAutoConstrainBuilder Class |
Represents a NXOpen.SketchAutoConstrainBuilder |
SketchAutoDimensionBuilder Class |
Represents a NXOpen.SketchAutoDimensionBuilder |
SketchChamferBuilder Class |
Represents a Chamfer builder |
SketchCollection Class |
Represents a collection of sketches |
SketchConicBuilder Class |
Represents a NXOpen.SketchConicBuilder builder |
SketchConstraint Class |
Represents a constraint in a sketch. |
SketchConstraintBuilder Class |
Represents a NXOpen.SketchConstraint builder |
SketchCornerBuilder Class |
Create a corner between two sketch curves. |
SketchDimensionBuilder Class |
Edit the geometry references of an existing sketch dimension. |
SketchDimensionalConstraint Class |
Represents a dimensional constraint |
SketchEditDefiningSectionBuilder Class |
Represents a NXOpen.SketchEditDefiningSectionBuilder builder. |
SketchEllipseBuilder Class |
Represents a NXOpen.SketchEllipseBuilder builder |
SketchEvaluator Class |
Represents a sketch-on-path evaluator. |
SketchEvaluatorCollection Class |
Represents a collection of NXOpen.SketchEvaluator . |
SketchExpressionModifierBuilder Class |
Represents a Sketch Expression Modifier Builder. |
SketchG1Constraint Class |
Represents a sketch G1 constraint |
SketchG2Constraint Class |
Represents a sketch G2 constraint |
SketchGeometricConstraint Class |
Represents a geometric sketch constraint |
SketchHelpedDimensionalConstraint Class |
Represents a dimensional sketch constraint that has a help point or help parameter |
SketchHelpedGeometricConstraint Class |
Represents a geometric sketch constraint that has a help point or help parameter |
SketchInDraftingBuilder Class |
Use the NXOpen.SketchInDraftingBuilder to create a NXOpen.Sketch on a NXOpen.Drawings.DraftingView or NXOpen.Drawings.DrawingSheet . |
SketchInPlaceBuilder Class |
Use the NXOpen.SketchInPlaceBuilder to create or reattach a NXOpen.Sketch on a NXOpen.DatumPlane or planar NXOpen.Face . |
SketchIntersectionCurve Class |
Represents a Intersection Curve operation inside sketch |
SketchIntersectionCurveBuilder Class |
Represents a NXOpen.SketchIntersectionCurve builder |
SketchIntersectionPoint Class |
Represents an Intersection Point operation inside sketch |
SketchIntersectionPointBuilder Class |
Represents a NXOpen.SketchIntersectionPoint builder |
SketchLinearDimensionBuilder Class |
Represents a NXOpen.SketchLinearDimensionBuilder |
SketchMakeSymmetricBuilder Class |
This class is used to add symmetric contraint to objects from a NXOpen.SketchMakeSymmetricBuilder . |
SketchMirrorBuilder Class |
This class is used to create a set of mirrored curves from a SketchMirrorBuilder . |
SketchMirrorPatternBuilder Class |
Represents a NXOpen.SketchMirrorPatternBuilder |
SketchOffset Class |
Represents a sketch offset constraint |
SketchOffsetBuilder Class |
Represents a NXOpen.SketchOffsetBuilder |
SketchPasteBuilder Class |
Represents a NXOpen.SketchPasteBuilder |
SketchPattern Class |
Represents a sketch pattern constraint |
SketchPatternBuilder Class |
Represents a NXOpen.SketchPatternBuilder |
SketchPolygon Class |
Represents a polygon constraint in a sketch |
SketchPolygonBuilder Class |
Represents a NXOpen.SketchPolygon builder |
SketchProjectBuilder Class |
Represents a NXOpen.SketchProjectBuilder builder |
SketchQuickExtendBuilder Class |
Represents a NXOpen.SketchQuickExtendBuilder |
SketchQuickTrimBuilder Class |
Represents a NXOpen.SketchQuickTrimBuilder |
SketchRadialDimensionBuilder Class |
Represents a NXOpen.SketchRadialDimensionBuilder |
SketchRapidDimensionBuilder Class |
Represents a NXOpen.SketchRapidDimensionBuilder |
SketchTangentConstraint Class |
Represents a tangent constraint |
SketchTangentToStringConstraint Class |
Represents a sketch tangent to string constraint |
SmartDiffValidator Class |
Implementation for Smart File Differencing |
SmartDiffValidatorBuilder Class |
Represents a SmartDiffValidator builder |
SmartObject Class |
Represents a smart object. |
SphericalCoordinateSystem Class |
Represents a spherical coordinate system |
Spline Class |
Represents a spline curve. |
SplineCollection Class |
Represents a collection of splines. |
Spreadsheet Class |
Represents a class for internal spreadsheet. |
SpreadsheetCellData Class |
Represents a class for Spreadsheet cell data. |
SpreadsheetExternal Class |
Represents a class for external spreadsheet. |
SpreadsheetManager Class |
Represents a class for interacting with spreadsheets. |
Step203Creator Class |
Represents a NXOpen.Step203Creator to be used when exporting the STEP203 Data This class is created using NXOpen.DexManager . |
Step203Importer Class |
Represents a NXOpen.Step203Importer to be used when importing the STEP203 Data This class is created using NXOpen.DexManager . |
Step214Creator Class |
Represents a NXOpen.Step214Creator to be used when exporting the STEP214 Data This class is created using NXOpen.DexManager . |
Step214Importer Class |
Represents a NXOpen.Step214Importer to be used when importing the STEP214 Data This class is created using NXOpen.DexManager . |
Step242Importer Class |
Represents a NXOpen.Step242Importer to be used when importing STEP242 Data This class is created using NXOpen.DexManager . |
StepCreator Class |
Represents a NXOpen.StepCreator to be used when exporting the STEP Data This class is created using NXOpen.DexManager . |
SubdivisionMeshBody Class |
Represents a subdivision mesh. |
SubdivisionMeshEdge Class |
Represents a subdivision mesh edge. |
SubdivisionMeshFace Class |
Represents a subdivision mesh face. |
SubdivisionMeshVertex Class |
Represents a subdivision mesh vertex. |
SubdivisionTaskEnvironment Class |
Represents the subdivision task environment associated with a session. |
SuppressByExpressionBuilder Class |
Represents a NXOpen.SuppressByExpressionBuilder |
SurfaceRebuildData Class |
Represents surface rebuild data structure. |
SurfaceUVDirectionBuilder Class |
Represents an edit surface u/v direction builder that allows reversing or swapping parametric directions. |
SymbolFont Class |
Represents a symbol font |
TableEditorDefaultDataProvider Class |
Provides basic data for a Table Editor block. |
TaggedObject Class |
Represents an object which has a Tag. |
TaggedObjectManager Class |
Represents a NXOpen.TaggedObjectManager |
TaggedObjectList Class |
Represents a list of objects. |
TextColorFontWidthBuilder Class |
Represent a NXOpen.TextColorFontWidthBuilder |
Traceline Class |
Represents a traceline. |
TracelineCollection Class |
Represents a collection of tracelines |
TransientObject Class |
Represents a base class for all NXOpen transient objects. |
TreeListNode Class |
Represents a TreeList Node Object |
UI Class |
This class contains the various elements that represent the NX User Interface. |
Unit Class |
Represents a unit |
UnitCollection Class |
Provides methods for manipulating the units in a part |
Update Class |
Provides methods for update and delete. |
VRMLImporter Class |
Used to import a VRML file into the work part. |
Validation Class |
Represents an NX NXOpen.Validation object. |
Validation3DSectionCollectionValidator Class |
validator for all drafting views |
ValidationAnnotation2DCollectionValidator Class |
validator for all 2d annotations in a part |
ValidationAnnotation3DCollectionValidator Class |
validator for all 3d annotations in a part |
ValidationAnnotationValidator Class |
annotation validator |
ValidationBaseArrowValidator Class |
validator for a Base Arrow |
ValidationBaseUserSymbolValidator Class |
validator for a user symbol |
ValidationBaseValidator Class |
Base validator drafting validation |
ValidationCenterLineValidator Class |
validator for a drafting centerline or center mark |
ValidationCollection Class |
Represents a collection of NXOpen.Validation . |
ValidationCoordinateNoteValidator Class |
validator for a Coordinate Note |
ValidationCurveCollectionValidator Class |
validator for drafting curves in a part |
ValidationCurveValidator Class |
validator for a drafting curve |
ValidationDatumTargetValidator Class |
validator for a datum target |
ValidationDatumValidator Class |
validator for a datum annotation |
ValidationDimensionValidator Class |
validator for a dimension |
ValidationDraftingEdgeVDCurveCollectionValidator Class |
validator for all drafting edge vdcurves in a part |
ValidationDraftingInterferenceVDCurveCollectionValidator Class |
validator for all drafting interference vdcurve in a part |
ValidationDraftingSectionEdgeVDCurveCollectionValidator Class |
validator for all drafting section edge vdcurves in a part |
ValidationDraftingSilhouetteVDCurveCollectionValidator Class |
validator for all drafting silhouette vdcurves in a part |
ValidationDraftingSimplifiedVDCurveCollectionValidator Class |
validator for all drafting simplified curves in a part |
ValidationDraftingThreadVDCurveCollectionValidator Class |
validator for all drafting thread(thread silhouette and thread section edge) vdcurves in a part |
ValidationDraftingTraceLineVDCurveCollectionValidator Class |
validator for all drafting traceline vdcurves in a part |
ValidationDraftingUVHatchVDCurveCollectionValidator Class |
validator for all drafting uvhatch vdcurve in a part |
ValidationDraftingVIVDCurveCollectionValidator Class |
validator for all drafting vi vdcurves in a part |
ValidationDrawingBookletValidator Class |
validator for a drafting member view |
ValidationDrawingRegionValidator Class |
validator for Drawing Region |
ValidationDrawingTo3DReportValidator Class |
validator for draw to 3d report |
ValidationDrawingTo3DValidator Class |
validator for all modeling views |
ValidationEnterpriseIdentificationValidator Class |
validator for a Enterprise Identification |
ValidationExtractedEdgeCollectionValidator Class |
validator for all drafting extracted edges in a part |
ValidationFcfValidator Class |
validator for a feature control frame |
ValidationFrameBarValidator Class |
validator for a FrameBar |
ValidationGeneralNoteValidator Class |
validator for a General Note |
ValidationHatchValidator Class |
validator for crosshatching |
ValidationHoleTableValidator Class |
validator for a Hole Table |
ValidationIdSymbolValidator Class |
validator for an id symbol |
ValidationInterferenceCurveCollectionValidator Class |
validator for all drafting interference curves in a part |
ValidationIntersectionSymbolValidator Class |
validator for a Intersection Symbol |
ValidationLabelOnParentValidator Class |
validator for a label on parent |
ValidationLayout2dComponentValidator Class |
validator for a layout2d component |
ValidationLocatorDesignatorValidator Class |
validator for a Locator Designator |
ValidationMaterialSpecificationValidator Class |
validator for a Material Specification |
ValidationMemberViewValidator Class |
validator for a drafting member view |
ValidationModelingViewSearchValidator Class |
validator for a modeling view |
ValidationModelingViewValidator Class |
validator for a modeling view |
ValidationModelingViewsCollectionValidator Class |
validator for all modeling views |
ValidationModelingViewsValidator Class |
validator for all modeling views |
ValidationNoteValidator Class |
validator for a note or label |
ValidationObjectCollectionValidator Class |
validator for a collection of drafting objects |
ValidationOffsetCenterPointSymbolValidator Class |
validator for a Offset Center Point Symbol |
ValidationPMIBalloonValidator Class |
validator for a PMI balloon note |
ValidationPMILightweightSectionViewValidator Class |
validator for a PMI Lightweight Section View |
ValidationPMIPlanarCPSValidator Class |
validator for a PMI Cutting Plate |
ValidationPMISectionViewValidator Class |
validator for a PMI Section View |
ValidationPartIdentificationValidator Class |
validator for a Part Identification |
ValidationPartListSectionValidator Class |
validator for a parts list section |
ValidationPartListValidator Class |
validator for a parts list |
ValidationProcessSpecificationValidator Class |
validator for a Process Specification |
ValidationRegionValidator Class |
validator for a Region |
ValidationSectionEdgesCollectionValidator Class |
validator for all section edges in a part |
ValidationSectionLineCollectionValidator Class |
validator for all section lines in a part |
ValidationSectionLineSegmentValidator Class |
validator for a section line segment |
ValidationSectionLineValidator Class |
validator for a section line |
ValidationSecurityMarkingValidator Class |
validator for a Security Marking |
ValidationSilhouetteCurveCollectionValidator Class |
validator for all drafting silhouette curves in a part |
ValidationSimplifiedCurveCollectionValidator Class |
validator for all drafting simplified curves in a part |
ValidationSpecificNoteValidator Class |
validator for a Specific Note |
ValidationSurfaceFinishValidator Class |
validator for a surface finish symbol |
ValidationSymbolValidator Class |
validator for a drafting symbol |
ValidationTabnotCollectionValidator Class |
validator for all tabnots |
ValidationTabnotSectionValidator Class |
validator for a Tabnot Section |
ValidationTabnotValidator Class |
validator for a tabnot |
ValidationTargetPointSymbolValidator Class |
validator for a Target Point Symbol |
ValidationThreadCurveCollectionValidator Class |
validator for all thread curves in a part |
ValidationThreadCurveValidator Class |
validator for a thread curve |
ValidationTitleBlockValidator Class |
validator for a Title Block |
ValidationTraceLineCollectionValidator Class |
validator for all drafting traceline curves in a part |
ValidationUVHatchCurveCollectionValidator Class |
validator for all drafting uvhatch curve in a part |
ValidationVDCurveValidator Class |
validator for a vdcurve |
ValidationVICurveCollectionValidator Class |
validator for all virtual intersection curves in a part |
ValidationViewBreakValidator Class |
validator for a section line |
ValidationViewCollectionValidator Class |
validator for all drafting views |
ValidationViewLabelValidator Class |
validator for a drawing view label |
ValidationViewValidator Class |
validator for a drafting view |
ValidationViewingDirectionArrowLabelValidator Class |
validator for a Viewing Direction Arrow Label |
ValidationViewingDirectionArrowValidator Class |
validator for a Viewing Direction Arrow |
ValidationWeldValidator Class |
validator for a dimension |
View Class |
Represents a view. |
ViewCollection Class |
Represents a collection of :py:class:`NXOpen.View`s. |
ViewDependentDisplayManager Class |
Represents all view dependent display operations |
WCS Class |
Represents the World Coordinate System. |
WidthDefinition Class |
Represents a NXOpen.WidthDefinition , which is a representation of an NX width palette. |
Xform Class |
Represents a smart xform |
XformCollection Class |
Represents a collection of NXOpen.Xform objects. |