ViewDependentDisplayManagerFont Enumeration

NXOpen.ViewDependentDisplayManager.Font is an alias for NXOpen.ViewDependentDisplayManagerFont

class NXOpen.ViewDependentDisplayManagerFont

Bases: object

specifies the font for wireframe edits

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
Invisible  
Solid  
Dashed  
Phantom  
Centerline  
Dotted  
LongDashed  
DottedDashed  
Object  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.