PartSaveStatus Class¶
-
class
NXOpen.
PartSaveStatus
¶ Bases:
NXOpen.TransientObject
This class represents a list of part names with associated status codes that serve to communicate why these parts where not able to be saved during part save.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
NumberUnsavedObjects | Returns the number of objects that could not be saved |
NumberUnsavedParts | Returns the number of parts that could not be saved |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetObjectStatus | Returns the error code indicating the reason the part could not be saved @return Error code reason that part could not be saved |
GetPart | Returns the name of a particular part that could not be saved @return |
GetStatus | Returns the error code indicating the reason the part could not be saved @return Error code reason that part could not be saved |
Property Detail¶
Method Detail¶
Dispose¶
-
PartSaveStatus.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetObjectStatus¶
-
PartSaveStatus.
GetObjectStatus
¶ Returns the error code indicating the reason the part could not be saved
Signature
GetObjectStatus(i)
Parameters: i (int) – Index into list of unsaved parts Returns: Error code reason that part could not be saved :rtype: int
New in version NX8.5.0.
License requirements: None.
GetPart¶
-
PartSaveStatus.
GetPart
¶ Returns the name of a particular part that could not be saved
Signature
GetPart(i)
Parameters: i (int) – Index into list of unsaved parts Returns: Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
GetStatus¶
-
PartSaveStatus.
GetStatus
¶ Returns the error code indicating the reason the part could not be saved
Signature
GetStatus(i)
Parameters: i (int) – Index into list of unsaved parts Returns: Error code reason that part could not be saved :rtype: int
New in version NX3.0.0.
License requirements: None.