HumanDataStatureType Enumeration¶
NXOpen.HumanData.StatureType is an alias for NXOpen.HumanDataStatureType
-
class
NXOpen.
HumanDataStatureType
¶ Bases:
object
This enum represents the stature data type of human
Enum Members
Enum Member Enum Member Description Percentile99 Indicate stature is 99% of populationPercentile95 Indicate stature is 95% of populationPercentile50 Indicate stature is 50% of populationPercentile5 Indicate stature is 5% of populationPercentile1 Indicate stature is 1% of populationCustom Indicate stature value is the actual height height of the humanRegress Indicate stature value is computed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-