LoadOptionsBookmarkRefsets Enumeration¶
NXOpen.LoadOptions.BookmarkRefsets is an alias for NXOpen.LoadOptionsBookmarkRefsets
-
class
NXOpen.
LoadOptionsBookmarkRefsets
¶ Bases:
object
the options that specify if reference set data from the bookmark should be restored and load should be optimized by loading topology from the selected reference sets only.
**Note:</b> The reference set data will only be restored for components that are part of the bookmark’s product assembly. The bookmark’s product assembly is the one that was the displayed part at the time the bookmark was saved.
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description ImportData Import reference set dataImportAndOptimizeLoad Import reference set data and use it to optimize loadDontImport Do nothing with the bookmark reference set data-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-