SelectionSelectionScope Enumeration¶
NXOpen.Selection.SelectionScope is an alias for NXOpen.SelectionSelectionScope
-
class
NXOpen.
SelectionSelectionScope
¶ Bases:
object
Indicates the scope for selecting objects.
Enum Members
Enum Member Enum Member Description UseDefault Use the default selection scopeWorkPart Use the work partAnyInAssembly Use any occurrence in the assemblyWorkPartAndOccurrence Use the work part or any occurrence-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-