ViewCollection Class¶
-
class
NXOpen.
ViewCollection
¶ Bases:
object
Represents a collection of :py:class:`NXOpen.View`s.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Property Detail¶
WorkView¶
-
ViewCollection.
WorkView
¶ Returns the work view of the part.
-------------------------------------
Getter Method
Signature
WorkView()
Returns: Work view Return type: NXOpen.View
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CreateBackground¶
-
ViewCollection.
CreateBackground
¶ Creates a
NXOpen.Display.Background
Signature
CreateBackground(view, makeReferencedObjects)
Parameters: - view (
NXOpen.View
) – view to which background data will be associated - makeReferencedObjects (bool) – true if referenced image object is to be created
Returns: Return type: New in version NX5.0.0.
License requirements: None.
- view (
CreateEnvironmentBuilder¶
-
ViewCollection.
CreateEnvironmentBuilder
¶ Creates a
NXOpen.Display.EnvironmentBuilder
Signature
CreateEnvironmentBuilder(view, makeReferencedObjects)
Parameters: - view (
NXOpen.View
) – view to which image-based lighting data will be associated - makeReferencedObjects (bool) – true if referenced image object is to be created
Returns: Return type: New in version NX10.0.2.
License requirements: studio_render (“UG STUDIO RENDER”)
- view (
CreateExtractScene¶
-
ViewCollection.
CreateExtractScene
¶ Creates a
NXOpen.Display.ExtractScene
Signature
CreateExtractScene(view)
Parameters: view ( NXOpen.View
) – view to which to extract the scene data will be associatedReturns: Return type: NXOpen.Display.ExtractScene
New in version NX5.0.0.
License requirements: None.
CreateGlobalIlluminationBuilder¶
-
ViewCollection.
CreateGlobalIlluminationBuilder
¶ Creates a
NXOpen.Display.GlobalIlluminationBuilder
Signature
CreateGlobalIlluminationBuilder()
Returns: Return type: NXOpen.Display.GlobalIlluminationBuilder
New in version NX9.0.0.
License requirements: None.
CreateImage¶
-
ViewCollection.
CreateImage
¶ Creates a
NXOpen.Display.Image
Signature
CreateImage(view)
Parameters: view ( NXOpen.View
) – view to which image data will be associatedReturns: Return type: NXOpen.Display.Image
New in version NX5.0.0.
License requirements: None.
CreateImageBasedLighting¶
-
ViewCollection.
CreateImageBasedLighting
¶ Creates a
NXOpen.Display.ImageBasedLighting
Signature
CreateImageBasedLighting(view, makeReferencedObjects)
Parameters: - view (
NXOpen.View
) – view to which image-based lighting data will be associated - makeReferencedObjects (bool) – true if referenced image object is to be created
Returns: Return type: New in version NX5.0.0.
License requirements: None.
- view (
CreateIrayPlusMaterialEditorBuilder¶
-
ViewCollection.
CreateIrayPlusMaterialEditorBuilder
¶ Creates a
NXOpen.Display.IrayPlusMaterialEditorBuilder
Signature
CreateIrayPlusMaterialEditorBuilder(materialName)
Parameters: materialName (str) – Returns: Return type: NXOpen.Display.IrayPlusMaterialEditorBuilder
New in version NX11.0.0.
License requirements: studio_render (“UG STUDIO RENDER”)
CreateIrayPlusSimpleMaterialEditorBuilder¶
-
ViewCollection.
CreateIrayPlusSimpleMaterialEditorBuilder
¶ Creates a
NXOpen.Display.IrayPlusSimpleMaterialEditorBuilder
Signature
CreateIrayPlusSimpleMaterialEditorBuilder()
Returns: Return type: NXOpen.Display.IrayPlusSimpleMaterialEditorBuilder
New in version NX10.0.2.
License requirements: studio_render (“UG STUDIO RENDER”)
CreateIrayPlusStudioEditorBuilder¶
-
ViewCollection.
CreateIrayPlusStudioEditorBuilder
¶ Creates a
NXOpen.Display.IRayPlusStudioEditorBuilder
Signature
CreateIrayPlusStudioEditorBuilder()
Returns: Return type: NXOpen.Display.IRayPlusStudioEditorBuilder
New in version NX10.0.2.
License requirements: studio_render (“UG STUDIO RENDER”)
CreateLightBuilder¶
-
ViewCollection.
CreateLightBuilder
¶ Creates a
NXOpen.Display.LightBuilder
Signature
CreateLightBuilder(light)
Parameters: light ( NXOpen.Light
) – light for which data will be modifiedReturns: Return type: NXOpen.Display.LightBuilder
New in version NX5.0.0.
License requirements: None.
CreateLighting¶
-
ViewCollection.
CreateLighting
¶ Creates a
NXOpen.Display.Lighting
Signature
CreateLighting(view)
Parameters: view ( NXOpen.View
) – view to which lighting data will be associatedReturns: Return type: NXOpen.Display.Lighting
New in version NX5.0.0.
License requirements: None.
CreateNonProportionalZoom¶
-
ViewCollection.
CreateNonProportionalZoom
¶ Creates a
NXOpen.Display.NonProportionalZoom
Signature
CreateNonProportionalZoom()
Returns: Return type: NXOpen.Display.NonProportionalZoom
New in version NX7.0.0.
License requirements: studio_analyze (“STUDIO ANALYZE”)
CreateRayTracedStudioBuilder¶
-
ViewCollection.
CreateRayTracedStudioBuilder
¶ Creates a
NXOpen.Display.RayTracedStudioBuilder
Signature
CreateRayTracedStudioBuilder()
Returns: Return type: NXOpen.Display.RayTracedStudioBuilder
New in version NX9.0.0.
License requirements: None.
CreateRayTracedStudioEditorBuilder¶
-
ViewCollection.
CreateRayTracedStudioEditorBuilder
¶ Creates a
NXOpen.Display.RayTracedStudioEditorBuilder
Signature
CreateRayTracedStudioEditorBuilder()
Returns: Return type: NXOpen.Display.RayTracedStudioEditorBuilder
New in version NX9.0.0.
License requirements: None.
CreateReflection¶
-
ViewCollection.
CreateReflection
¶ Creates a
NXOpen.Display.Reflection
Signature
CreateReflection(view, makeReferencedObjects)
Parameters: - view (
NXOpen.View
) – view to which reflection data will be associated - makeReferencedObjects (bool) – true if referenced image object is to be created
Returns: Return type: New in version NX5.0.0.
License requirements: None.
- view (
CreateSaveImageFileBrowserBuilder¶
-
ViewCollection.
CreateSaveImageFileBrowserBuilder
¶ Creates a
NXOpen.Display.SaveImageFileBrowserBuilder
Signature
CreateSaveImageFileBrowserBuilder()
Returns: Return type: NXOpen.Display.SaveImageFileBrowserBuilder
New in version NX9.0.0.
License requirements: None.
CreateScene¶
-
ViewCollection.
CreateScene
¶ Creates a
NXOpen.Display.Scene
Signature
CreateScene(view, makeReferencedObjects)
Parameters: - view (
NXOpen.View
) – view to which scene data will be associated - makeReferencedObjects (bool) – true if scene objects are to be created
Returns: Return type: New in version NX5.0.0.
License requirements: None.
- view (
CreateShadows¶
-
ViewCollection.
CreateShadows
¶ Creates a
NXOpen.Display.Shadows
Signature
CreateShadows(view)
Parameters: view ( NXOpen.View
) – view to which shadows data will be associatedReturns: Return type: NXOpen.Display.Shadows
New in version NX7.5.3.
License requirements: None.
CreateStage¶
-
ViewCollection.
CreateStage
¶ Creates a
NXOpen.Display.Stage
Signature
CreateStage(view, makeReferencedObjects)
Parameters: - view (
NXOpen.View
) – view to which stage data will be associated - makeReferencedObjects (bool) – true if first wall’s image object is to be created
Returns: Return type: New in version NX5.0.0.
License requirements: None.
- view (
CreateStudioImageCaptureBuilder¶
-
ViewCollection.
CreateStudioImageCaptureBuilder
¶ Creates a
NXOpen.Display.StudioImageCaptureBuilder
Signature
CreateStudioImageCaptureBuilder()
Returns: Return type: NXOpen.Display.StudioImageCaptureBuilder
New in version NX6.0.4.
License requirements: None.
CreateWall¶
-
ViewCollection.
CreateWall
¶ Creates a
NXOpen.Display.Wall
Signature
CreateWall(view, wallType)
Parameters: - view (
NXOpen.View
) – view to which stage data will be associated - wallType – where the wall sits in the Display.
Stage :type wallType:
NXOpen.Display.StageWallType
:returns: :rtype:NXOpen.Display.Wall
New in version NX5.0.0.
License requirements: None.
- view (
FindObject¶
-
ViewCollection.
FindObject
¶ Finds the
NXOpen.View
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the view to be found Returns: View with this identifier Return type: NXOpen.View
New in version NX3.0.0.
License requirements: None.
FitAll¶
-
ViewCollection.
FitAll
¶ Adjusts the center and scale of each view in the current layout such that all of each view is visible, except that this fit operation is not applied to member views on a drawing.
If the work view is in expand state when this method is called, the work view is unexpanded before all of the views are fit.
In batch mode, the data for each view is updated, but no display occurs.
Signature
FitAll()
New in version NX4.0.0.
License requirements: None.
GetActiveViews¶
-
ViewCollection.
GetActiveViews
¶ Returns the active views in the view collection.
Signature
GetActiveViews()
Returns: List of active views Return type: list of NXOpen.View
New in version NX3.0.0.
License requirements: None.
GetCustomViews¶
-
ViewCollection.
GetCustomViews
¶ Returns a list of custom view names in the view collection.
Signature
GetCustomViews()
Returns: List of custom view names Return type: list of str New in version NX3.0.0.
License requirements: None.
IsWorkViewExpanded¶
-
ViewCollection.
IsWorkViewExpanded
¶ Returns whether the work view of the given part is in expand state.
Signature
IsWorkViewExpanded()
Returns: true if the work view is expanded Return type: bool New in version NX4.0.0.
License requirements: None.
Refresh¶
-
ViewCollection.
Refresh
¶ Refreshes all the views in the current layout
Signature
Refresh()
New in version NX3.0.0.
License requirements: None.
Regenerate¶
-
ViewCollection.
Regenerate
¶ Regenerates the display of each view in the current layout.
The current scale of each view is used in determing the tolerances for rendering curves and facets within the view.
In batch mode, the state of each view is updated, but no display occurs.
Signature
Regenerate()
New in version NX4.0.0.
License requirements: None.
Save¶
-
ViewCollection.
Save
¶ Saves current view.
Signature
Save()
New in version NX3.0.0.
License requirements: None.
SaveAs¶
-
ViewCollection.
SaveAs
¶ Saves a view with user specified name.
Signature
SaveAs(selectedView, newViewName, copyViewModifications, moveViewDependencies)
Parameters: - selectedView (
NXOpen.View
) – Selected view - newViewName (str) – Selected name of the view
- copyViewModifications (bool) – True if view modifications to be copied
- moveViewDependencies (bool) – True if view dependencies to be moved
Returns: Newly created view
Return type: New in version NX3.0.0.
License requirements: None.
- selectedView (
SaveAsPreservingCase¶
-
ViewCollection.
SaveAsPreservingCase
¶ Preserve case for user defined view names.
Signature
SaveAsPreservingCase(selectedView, newViewName, copyViewModifications, moveViewDependencies)
Parameters: - selectedView (
NXOpen.View
) – Selected view - newViewName (str) – Selected name of the view
- copyViewModifications (bool) – True if view modifications to be copied
- moveViewDependencies (bool) – True if view dependencies to be moved
Returns: Newly created view
Return type: New in version NX8.0.0.
License requirements: None.
- selectedView (
UnexpandWork¶
-
ViewCollection.
UnexpandWork
¶ Removes the work view from the expand state (assuming that it is in that state), restoring it to its normal size in its layout.
Other views in the layout become visible again. If the work view is not in expand state, an error is returned. The view remains the work view unless the view is a member view on a drawing sheet, in which case the sheet’s view becomes the work view. The given part must be the displayed part.
In batch mode, the internal state of the view is no longer in expand state, but no display occurs.
Signature
UnexpandWork()
New in version NX4.0.0.
License requirements: None.
UpdateDisplay¶
-
ViewCollection.
UpdateDisplay
¶ Updates the display of each view in the current layout.
This method redisplays those objects whose display has become out of date due to rotations of the view or increases in view scale. For example: Following a rotation, the silhouettes of bodies in wireframe mode will be updated; Following a significant scale increase, the faces of a body in shaded mode will be tessalated with tighter tolerances.
In batch mode, the state of each view is updated, but no display occurs.
Signature
UpdateDisplay()
New in version NX4.0.0.
License requirements: None.