ExtractScene Class¶
-
class
NXOpen.Display.
ExtractScene
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.ExtractScene
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateExtractScene()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
SceneName | Returns or sets the scene name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSceneDescription | Returns the scene description @return |
ImageFileSelect | Gets an image file using file selection. |
Information | The scene information |
SetSceneDescription | Sets the scene description |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SceneName¶
-
ExtractScene.
SceneName
¶ Returns or sets the scene name
-------------------------------------
Getter Method
Signature
SceneName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SceneName(sceneName)
Parameters: sceneName (str) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetSceneDescription¶
-
ExtractScene.
GetSceneDescription
¶ Returns the scene description
Signature
GetSceneDescription()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
ImageFileSelect¶
-
ExtractScene.
ImageFileSelect
¶ Gets an image file using file selection.
Signature
ImageFileSelect()
New in version NX5.0.0.
License requirements: None.
Information¶
-
ExtractScene.
Information
¶ The scene information
Signature
Information()
New in version NX5.0.0.
License requirements: None.
SetSceneDescription¶
-
ExtractScene.
SetSceneDescription
¶ Sets the scene description
Signature
SetSceneDescription(sceneDescription)
Parameters: sceneDescription (list of str) – New in version NX5.0.0.
License requirements: None.
Validate¶
-
ExtractScene.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.