SaveImageFileBrowserBuilder Class¶
-
class
NXOpen.Display.
SaveImageFileBrowserBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.SaveImageFileBrowserBuilder
.Saves an image file using a file browser.
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateSaveImageFileBrowserBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FileFormat | Returns or sets the Ray Traced Studio static image file format |
NativeImageFileBrowser | Returns or sets the Ray Traced Studio static image file browser |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SaveImageFileBrowserBuilderFileFormats Enumeration | To specify the Ray Traced Studio static image file format |
Property Detail¶
FileFormat¶
-
SaveImageFileBrowserBuilder.
FileFormat
¶ Returns or sets the Ray Traced Studio static image file format
-------------------------------------
Getter Method
Signature
FileFormat()
Returns: Return type: NXOpen.Display.SaveImageFileBrowserBuilderFileFormats
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileFormat(fileFormat)
Parameters: fileFormat ( NXOpen.Display.SaveImageFileBrowserBuilderFileFormats
) –New in version NX9.0.0.
License requirements: None.
NativeImageFileBrowser¶
-
SaveImageFileBrowserBuilder.
NativeImageFileBrowser
¶ Returns or sets the Ray Traced Studio static image file browser
-------------------------------------
Getter Method
Signature
NativeImageFileBrowser()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NativeImageFileBrowser(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SaveImageFileBrowserBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.