Lighting Class¶
-
class
NXOpen.Display.
Lighting
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Display.Lighting
Lights are used to illuminate the scene in Shaded and Studio rendering styles, as well as in High Quality Images.This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To create a new instance of this class, use
NXOpen.ViewCollection.CreateLighting()
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetLightBuilderFromList | Returns a light builder, given by the index, in the array of lights assigned to the work view @return the light builder |
GetNumLightBuilders | Returns the total number of light builders in the given lighting list @return total lights in the light builder array |
GetObject | Returns the object currently being edited by this builder. |
SetLightBuilderInList | Sets a light builder in the array at the given index |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetLightBuilderFromList¶
-
Lighting.
GetLightBuilderFromList
¶ Returns a light builder, given by the index, in the array of lights assigned to the work view
Signature
GetLightBuilderFromList(index)
Parameters: index (int) – index to the array of light builders Returns: the light builder Return type: NXOpen.Display.LightBuilder
New in version NX5.0.0.
License requirements: None.
GetNumLightBuilders¶
-
Lighting.
GetNumLightBuilders
¶ Returns the total number of light builders in the given lighting list
Signature
GetNumLightBuilders()
Returns: total lights in the light builder array Return type: int New in version NX5.0.0.
License requirements: None.
SetLightBuilderInList¶
-
Lighting.
SetLightBuilderInList
¶ Sets a light builder in the array at the given index
Signature
SetLightBuilderInList(index, light)
Parameters: - index (int) – index to the array of light builders
- light (
NXOpen.Display.LightBuilder
) – the light builder
New in version NX5.0.0.
License requirements: None.
Validate¶
-
Lighting.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.