ViewDependentDisplayManagerTranslucency Enumeration

NXOpen.ViewDependentDisplayManager.Translucency is an alias for NXOpen.ViewDependentDisplayManagerTranslucency

class NXOpen.ViewDependentDisplayManagerTranslucency

Bases: object

specifies the translucency options for shading edits

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
NoChange  
Original  
Yes  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.