LayoutDefinitionArrangementType Enumeration¶
NXOpen.LayoutDefinition.ArrangementType is an alias for NXOpen.LayoutDefinitionArrangementType
-
class
NXOpen.
LayoutDefinitionArrangementType
¶ Bases:
object
Indicates the arrangement type of a layout.
New in version NX3.0.0.
Enum Members
A layout definition cannot be made with this option. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-