MovieSettingsBuilderPlaybackSpeedChoices Enumeration¶
NXOpen.MovieSettingsBuilder.PlaybackSpeedChoices is an alias for NXOpen.MovieSettingsBuilderPlaybackSpeedChoices
-
class
NXOpen.
MovieSettingsBuilderPlaybackSpeedChoices
¶ Bases:
object
Indicates the playback speed of the movie.
Enum Members
Enum Member Enum Member Description VerySlow Specifies very slow playback speed (quarter of record speed)Slow Specifies slow playback speed (half of record speed)AsRecorded Specifies playback speed same as record speedFast Specifies fast playback speed (twice record speed)VeryFast Specifies very fast playback speed (four times record speed)-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-