PhysicalMaterialType Enumeration¶
NXOpen.PhysicalMaterial.Type is an alias for NXOpen.PhysicalMaterialType
-
class
NXOpen.
PhysicalMaterialType
¶ Bases:
object
The different types of materials.
The material list generated will be filtered based on the material type chosen
Enum Members
Enum Member Enum Member Description Unknown unknown == errorIsotropic IsotropicOrthotropic OrthotropicAnisotropic AnisotropicFluid FluidGeneralHyperelastic Hyperelastic - GeneralMooneyrivlin Mooney RivlinMooneyrivlintestdata Mooney Rivlin - test data optionPolynomial PolynomialReducedpolynomial Reduced PolynomialOgden OgdenOgdentestdata Ogden - test data optionFoam FoamFoamtestdata Foam - test data optionBlatz Blatz-KoArrudaboyce Arruda-BoyceArrudaboycetestdata Arruda-Boyce - test data optionNeohooke Neo HookeNeohooketestdata Neo Hooke - test data optionMarlow MarlowVanderwaals Van Der WaalsYeoh YeohYeohtestdata Yeoh - test data optionGent GentGasket GasketGasketbehavior Gasket BehaviorShapememoryalloy Shape Memory AlloySussmanbathe Sussman-Bathe hyperelastic materialGasketdisplacement Gasket with length-based loadingDamageinterface Damage interface materialMultiplefluid Multiple fluid materialHartsmith Hart-Smith materialAlexander Alexander materialCuring Curing materialPorous Porous material-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-