LineCollection Class¶
-
class
NXOpen.
LineCollection
¶ Bases:
object
Represents a collection of lines.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateFaceAxis | Create a Axis line base on a Cylider, Cone, Torus or Revolve face @return |
CreateFaceAxisNoExtension | Create a Axis line base on a Cylider, Cone, Torus or Revolve face. |
CreateFaceAxisNoParentLoadRequired | Create a Axis line base on a Cylider, Cone, Torus or Revolve face. |
FindObject | Finds the NXOpen.Line with the given identifier as recorded in a journal. |
Method Detail¶
CreateFaceAxis¶
-
LineCollection.
CreateFaceAxis
¶ Create a Axis line base on a Cylider, Cone, Torus or Revolve face
Signature
CreateFaceAxis(face, updateOption)
Parameters: - face (
NXOpen.IParameterizedSurface
) – face - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- face (
CreateFaceAxisNoExtension¶
-
LineCollection.
CreateFaceAxisNoExtension
¶ Create a Axis line base on a Cylider, Cone, Torus or Revolve face.
Do not extend the line.
Signature
CreateFaceAxisNoExtension(face, updateOption)
Parameters: - face (
NXOpen.IParameterizedSurface
) – face - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- face (
CreateFaceAxisNoParentLoadRequired¶
-
LineCollection.
CreateFaceAxisNoParentLoadRequired
¶ Create a Axis line base on a Cylider, Cone, Torus or Revolve face.
If the parent (source) part is not the same part that the axis is created in, the parent part is not fully loaded during the creation.
Signature
CreateFaceAxisNoParentLoadRequired(face, updateOption)
Parameters: - face (
NXOpen.IParameterizedSurface
) – face - updateOption (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- face (
FindObject¶
-
LineCollection.
FindObject
¶ Finds the
NXOpen.Line
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the line Returns: Return type: NXOpen.Line
New in version NX3.0.0.
License requirements: None.