SmartObjectUpdateOption Enumeration¶
NXOpen.SmartObject.UpdateOption is an alias for NXOpen.SmartObjectUpdateOption
-
class
NXOpen.
SmartObjectUpdateOption
¶ Bases:
object
Specifies when the smart object updates.
Enum Members
Enum Member Enum Member Description DontUpdate No update occurs.WithinModeling Updates within modeling (e.g. a feature).AfterModeling Updates after modeling (e.g. a dimension).AfterParentBody Updates after the parent body.Mixed Updates after parent body for inter-part parents and updates within modeling for same part parents-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-