AutomaticTracelineModeOption Enumeration¶
NXOpen.AutomaticTraceline.ModeOption is an alias for NXOpen.AutomaticTracelineModeOption
-
class
NXOpen.
AutomaticTracelineModeOption
¶ Bases:
object
Controls the mode used when evaluating an automatic traceline
Enum Members
Enum Member Enum Member Description Evaluate Evaluate which mode to useOrientation Align with orientationInfer Infer orientation from start and end directions-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-