SketchAutoDimensioningRule Enumeration¶
NXOpen.Sketch.AutoDimensioningRule is an alias for NXOpen.SketchAutoDimensioningRule
-
class
NXOpen.
SketchAutoDimensioningRule
¶ Bases:
object
Type of Auto Dimensioning rules.
It should match the rule types defined in Auto Dimensioning engine. Auto Dimensioning rules affect how the dimensions are created by the Auto Dimensioner. The rules will be put in a list, the first the rule with the highest priority and the last rule with the lowest priority. The user can change the order of the rules in the list to persue the flavor of the dimensions he wants.
NXOpen.SketchAutoDimensioningRule.Symmetric
: create symmetric dimensions if the curves are symmetricNXOpen.SketchAutoDimensioningRule.AdjacentAngle
: create angles between adjacent linesNXOpen.SketchAutoDimensioningRule.Length
: create length dimension for linesNXOpen.SketchAutoDimensioningRule.HorizontalVertical
: create horizontal and vertical dimensionsNXOpen.SketchAutoDimensioningRule.ReferenceAxes
: create dimensions between curves and reference axesEnum Members
Enum Member Enum Member Description Symmetric Create Symmetric DimensionsAdjacentAngle Create Adjacent AnglesLength Create Length DimensionHorizontalVertical Create Horizontal and Vertical DimensionsReferenceAxes Create Dimensions to Reference Axes-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-