ValidationResult Enumeration¶
NXOpen.Validation.Result is an alias for NXOpen.ValidationResult
-
class
NXOpen.
ValidationResult
¶ Bases:
object
Specifies result of the validation
Enum Members
Enum Member Enum Member Description Pass Validation Pass all checksInformation Validation Pass with informationWarning Validation Pass with warningFailed Validation FailedUnknown Unknown validation resultSkipped Validation Skipped-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-