DisplayManager Class¶
-
class
NXOpen.
DisplayManager
¶ Bases:
object
Represents an object to manage display settings.
Input to this class can be PSM facet objects. To obtain an instance of this class, refer to
NXOpen.Session
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
FacetCacheMemoryLevel | Returns or sets the memory level of the display facet cache system. |
Methods¶
Method | Description |
---|---|
BlankObjects | Blank a set of displayable objects. |
GetJ3dData | Returns the list of displayable entities along with display information for each entity in the displayed part. |
GetJ3dGeometry | Returns polygon/vector information for an entity @return true if vector data produced |
GetShowableHideableTypes | Returns an array of all Registered ShowHideType strings. |
HideByType | Hides a set of objects by type. |
MakeUpToDate | Ensures that previously invoked display operations are complete. |
NewDisplayModification | Constructs a new NXOpen.DisplayModification object. |
ShowAdjacent | Display objects adjacent to a set of displayable objects(NXOpen.CAE.CAEFace , NXOpen.CAE.CAEEdge ). |
ShowByType | Shows a set of objects by type. |
ShowNodesRelatedToDisplayedElements | Display all nodes related to displayed elements. |
ShowObjects | Unblank a set of displayable objects considering the following layer settings if the objects are in invisible layers. |
ShowOnly | Show a set of displayable objects. |
UnblankObjects | Unblank a set of displayable objects. |
Enumerations¶
DisplayManagerFacetCacheMemoryLevelType Enumeration | Facet cache memory level. |
DisplayManagerLayerSetting Enumeration | Represents the layer settings when the objects to show are in invisible layers |
DisplayManagerShowHideScope Enumeration | Controls the scope for the show hide operation. |
DisplayManagerShowHideType Enumeration | Controls the type of object to show or hide. |
Structs¶
DisplayManagerJ3dColor_Struct Struct | 3d interface color definition |
DisplayManagerJ3dData_Struct Struct | 3d interface structure |
DisplayManagerJ3dMaterial_Struct Struct | 3d interface material definition |
Property Detail¶
FacetCacheMemoryLevel¶
-
DisplayManager.
FacetCacheMemoryLevel
¶ Returns or sets the memory level of the display facet cache system.
Facet cache memory level is used to manage the memory footprint of the display facet cache. Higher memory level implies higher memory footprint.
Facet caching can be turned off by setting the memory level to
NXOpen.DisplayManagerFacetCacheMemoryLevelType.None
. For all other memory levels, the display system will attempt to perform periodic cleanup if it detects that NX is experiencing memory pressure. The extent of cleanup depends on the memory level. Lower memory level indicates that more cleanup is desired to keep loweer memory footprint. Note that low memory level can slow down rendering performance due to absence of facet data in the facet cache.-------------------------------------
Getter Method
Signature
FacetCacheMemoryLevel()
Returns: Return type: NXOpen.DisplayManagerFacetCacheMemoryLevelType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FacetCacheMemoryLevel(memoryLevel)
Parameters: memoryLevel ( NXOpen.DisplayManagerFacetCacheMemoryLevelType
) –New in version NX10.0.0.
License requirements: None.
Method Detail¶
BlankObjects¶
-
DisplayManager.
BlankObjects
¶ Blank a set of displayable objects.
You may want to use
NXOpen.View.FitAfterShowOrHide()
after using this method. Some displayable objects are not valid for this method and, if found in the objects input, will be ignored. These include face and edge objects of solid bodies.Signature
BlankObjects(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX3.0.0.
License requirements: None.
GetJ3dData¶
-
DisplayManager.
GetJ3dData
¶ Returns the list of displayable entities along with display information for each entity in the displayed part.
Signature
GetJ3dData()
Returns: Array of entities and display data Return type: list of NXOpen.DisplayManagerJ3dData_Struct
New in version NX5.0.0.
License requirements: None.
GetJ3dGeometry¶
-
DisplayManager.
GetJ3dGeometry
¶ Returns polygon/vector information for an entity
Signature
GetJ3dGeometry(eid, tolerance, wireframe)
Parameters: - eid (
NXOpen.DisplayableObject
) – entity to tesselate - tolerance (float) – adjustment factor for tesselation tolerance
- wireframe (bool) – if true generates wireframe solids
Returns: a tuple
Return type: A tuple consisting of (vectors, points, normals, pointsPerStrip). vectors is a bool. true if vector data produced points is a list of float. polygon/vector points normals is a list of float. polygon normals pointsPerStrip is a list of int. points for each triangle strip
New in version NX5.0.0.
License requirements: None.
- eid (
GetShowableHideableTypes¶
-
DisplayManager.
GetShowableHideableTypes
¶ Returns an array of all Registered ShowHideType strings.
Signature
GetShowableHideableTypes()
Returns: Registered ShowHideType strings. Return type: list of str New in version NX9.0.0.
License requirements: None.
HideByType¶
-
DisplayManager.
HideByType
¶ Overloaded method HideByType
HideByType(type, scope)
HideByType(type, scope)
-------------------------------------
Hides a set of objects by type. You may want to use
NXOpen.View.FitAfterShowOrHide()
after using this method.Signature
HideByType(type, scope)
Parameters: - type (
NXOpen.DisplayManagerShowHideType
) – The type of object to hide - scope (
NXOpen.DisplayManagerShowHideScope
) – The scope for the show hide operation
Returns: The number of objects hidden
Return type: int
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.DisplayManager.HideByType()
that takes a string type instead. To find all registered ShowHideType string useNXOpen.DisplayManager.GetShowableHideableTypes()
License requirements: None.
-------------------------------------
Hides a set of objects by type. You may want to use
NXOpen.View.FitAfterShowOrHide()
after using this method.Signature
HideByType(type, scope)
Parameters: - type (str) – The type of object to hide
- scope (
NXOpen.DisplayManagerShowHideScope
) – The scope for the show hide operation
Returns: The number of objects hidden
Return type: int
New in version NX9.0.0.
License requirements: None.
-------------------------------------
MakeUpToDate¶
-
DisplayManager.
MakeUpToDate
¶ Ensures that previously invoked display operations are complete.
Called only by NXOpen applications that directly invoke Windows, MFC, or Motif functions to display dialogs. This function is not needed when NXOpen dialogs are used.
Signature
MakeUpToDate()
New in version NX3.0.0.
License requirements: None.
NewDisplayModification¶
-
DisplayManager.
NewDisplayModification
¶ Constructs a new
NXOpen.DisplayModification
object.Signature
NewDisplayModification()
Returns: The new DisplayModification instance Return type: NXOpen.DisplayModification
New in version NX3.0.0.
License requirements: None.
ShowAdjacent¶
-
DisplayManager.
ShowAdjacent
¶ Display objects adjacent to a set of displayable objects(
NXOpen.CAE.CAEFace
,NXOpen.CAE.CAEEdge
).If
NXOpen.CAE.CAEFace
selected, display all it’s neighbouring faces and associated edges. IfNXOpen.CAE.CAEEdge
selected, display it’s associated faces and their associated edges.Signature
ShowAdjacent(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ShowByType¶
-
DisplayManager.
ShowByType
¶ Overloaded method ShowByType
ShowByType(type, scope)
ShowByType(type, scope)
-------------------------------------
Shows a set of objects by type. You may want to use
NXOpen.View.FitAfterShowOrHide()
after using this method.Signature
ShowByType(type, scope)
Parameters: - type (
NXOpen.DisplayManagerShowHideType
) – The type of object to show - scope (
NXOpen.DisplayManagerShowHideScope
) – The scope for the show hide operation
Returns: The number of objects shown
Return type: int
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.DisplayManager.ShowByType()
that takes a string type instead.License requirements: None.
-------------------------------------
Shows a set of objects by type. You may want to use
NXOpen.View.FitAfterShowOrHide()
after using this method.Signature
ShowByType(type, scope)
Parameters: - type (str) – The type of object to show
- scope (
NXOpen.DisplayManagerShowHideScope
) – The scope for the show hide operation
Returns: The number of objects shown
Return type: int
New in version NX9.0.0.
License requirements: None.
-------------------------------------
ShowObjects¶
-
DisplayManager.
ShowObjects
¶ Unblank a set of displayable objects considering the following layer settings if the objects are in invisible layers.
NXOpen.DisplayManagerLayerSetting.MoveObjectsToWorkLayer
- The objects will be moved to work layer before unblanking the objects if they are in invisible layer.NXOpen.DisplayManagerLayerSetting.ChangeLayerToSelectable
- The objects layer will be changed to selectable if the layer is invisible
Signature
ShowObjects(objects, layerSetting)
Parameters: - objects (list of
NXOpen.DisplayableObject
) – - layerSetting (
NXOpen.DisplayManagerLayerSetting
) – Layer setting option
New in version NX5.0.2.
License requirements: None.
ShowOnly¶
-
DisplayManager.
ShowOnly
¶ Show a set of displayable objects.
The objects selectable are:
NXOpen.Curve
,NXOpen.Point
,NXOpen.CAE.MeshPoint
, CSYS,NXOpen.Plane
, Mesh,NXOpen.CAE.CAEBody
,NXOpen.CAE.CAEFace
, Load, Constraint and Simulation Object. You may want to useNXOpen.View.FitAfterShowOrHide()
after using this method.Signature
ShowOnly(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UnblankObjects¶
-
DisplayManager.
UnblankObjects
¶ Unblank a set of displayable objects.
You may want to use
NXOpen.View.FitAfterShowOrHide()
after using this method. Some displayable objects are not valid for this method and, if found in the objects input, will be ignored. These include face and edge objects of solid bodies.Signature
UnblankObjects(objects)
Parameters: objects (list of NXOpen.DisplayableObject
) –New in version NX3.0.0.
License requirements: None.