DisplayManagerLayerSetting Enumeration¶
NXOpen.DisplayManager.LayerSetting is an alias for NXOpen.DisplayManagerLayerSetting
-
class
NXOpen.
DisplayManagerLayerSetting
¶ Bases:
object
Represents the layer settings when the objects to show are in invisible layers
Enum Members
Enum Member Enum Member Description MoveObjectsToWorkLayer Move the objects to work layer if they are in invisible layerChangeLayerToSelectable Change the layer to selectable if it is invisibleInvalid Last value, should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-