UI Class¶
-
class
NXOpen.
UI
¶ Bases:
NXOpen.TaggedObject
This class contains the various elements that represent the NX User Interface.
There is a single instance of this class per session. To obtain a reference to the current UI, call the static method
UI.GetUI()
.For Java, use <code>SessionFactory::get(“UI”)</code> to obtain the reference of the current UI.
For language bindings that support remoting, the server must export it for this class to be obtained by a client.
Use the static method in this class to obtain an instance.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
NXMessageBox |
|
Styler |
|
SelectionManager |
|
ObjectPreferences |
|
UserInterfacePreferences |
|
VisualizationVisualPreferences |
|
VisualizationLinePreferences |
|
VisualizationShadingPreferences |
|
MenuBarManager |
|
MovieManager |
|
ResourceBarManager |
|
Methods¶
Method | Description |
---|---|
AddUtilityFunctionVisibilityHandler | Registers a user defined method that is called whenever an utility function state changes. |
AskLockStatus | Query NX lock status. |
CanOpenPart | Returns a flag indicating whether the NX user interface is in a state where opening a part and making it the display part is supported. |
CreateCustomPopupMenuHandler | Create a custom menu. |
CreateDialog | Creates a block dialog. |
JournalPause | Pauses execution of a journal. |
LockAccess | Locks access to the NX User Interface. |
RemoveUtilityFunctionVisibilityHandler | Unregisters a user defined method that is called whenever an utility function state changes. |
UnlockAccess | Unlocks access for a UI that has been locked by a call to LockAccess() . |
Enumerations¶
UIStatus Enumeration | Indicates the Lock, Unlock status of NX functions. |
NXMessageBox¶
-
UI.
NXMessageBox
¶ the Uistyler for the current session.
Signature
NXMessageBox()
New in version NX3.0.0.
Returns: Return type: NXOpen.NXMessageBox
Styler¶
-
UI.
Styler
¶ the Uistyler for the current session.
Signature
Styler()
New in version NX3.0.0.
Returns: Return type: NXOpen.UIStyler.Styler
SelectionManager¶
-
UI.
SelectionManager
¶ the SelectionManager for the current session.
Signature
SelectionManager()
New in version NX3.0.0.
Returns: Return type: NXOpen.Selection
ObjectPreferences¶
-
UI.
ObjectPreferences
¶ the UI based Object Preferences in the current session.
Signature
ObjectPreferences()
New in version NX3.0.0.
Returns: Return type: NXOpen.Preferences.ObjectPreferences
UserInterfacePreferences¶
-
UI.
UserInterfacePreferences
¶ the UI based User Interface Preferences in the current session
Signature
UserInterfacePreferences()
New in version NX3.0.0.
Returns: Return type: NXOpen.Preferences.SessionUserInterfaceUI
VisualizationVisualPreferences¶
-
UI.
VisualizationVisualPreferences
¶ the UI based Visualization Preferences under Visual Tab in the current session
Signature
VisualizationVisualPreferences()
New in version NX3.0.0.
Returns: Return type: NXOpen.Preferences.SessionVisualizationVisual
VisualizationLinePreferences¶
-
UI.
VisualizationLinePreferences
¶ the UI based Visualization Preferences under Line Tab in the current session
Signature
VisualizationLinePreferences()
New in version NX3.0.0.
Returns: Return type: NXOpen.Preferences.VisualizationLine
VisualizationShadingPreferences¶
-
UI.
VisualizationShadingPreferences
¶ the UI based Visualization Preferences under Shading Tab in the current session
Signature
VisualizationShadingPreferences()
New in version NX3.0.0.
Returns: Return type: NXOpen.Preferences.SessionVisualizationShade
MovieManager¶
-
UI.
MovieManager
¶ the Movie Manager class.
Signature
MovieManager()
New in version NX3.0.0.
Returns: Return type: NXOpen.MovieManager
ResourceBarManager¶
Method Detail¶
AddUtilityFunctionVisibilityHandler¶
-
UI.
AddUtilityFunctionVisibilityHandler
¶ Registers a user defined method that is called whenever an utility function state changes.
Signature
AddUtilityFunctionVisibilityHandler(utilityFunctionVisibilityHandler)
Parameters: utilityFunctionVisibilityHandler (CallableObject) – Returns: identifier of registered method (used to unregister the method) Return type: int New in version NX5.0.5.
License requirements: None.
AskLockStatus¶
-
UI.
AskLockStatus
¶ Query NX lock status.
This function is useful when dismissing a custom dialog and you want to determine whether or not a lock has been set. Returns :py:class:` UIStatus.Lock < UIStatus>`, when NX is in lock status. Returns :py:class:` UIStatus.Unlock < UIStatus>`, when NX is in unlock status.
Signature
AskLockStatus()
Returns: Return type: NXOpen.UIStatus
New in version NX5.0.0.
License requirements: None.
CanOpenPart¶
-
UI.
CanOpenPart
¶ Returns a flag indicating whether the NX user interface is in a state where opening a part and making it the display part is supported.
For example if certain dialogs are displayed or the system is in a task environment it is not supported
Signature
CanOpenPart()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
CreateDialog¶
-
UI.
CreateDialog
¶ Creates a block dialog.
Use <code>#undef CreateDialog</code> in C++ programs to avoid confusion with Windows API
Signature
CreateDialog(dialogName)
Parameters: dialogName (str) – Dialog name Returns: Return type: NXOpen.BlockStyler.BlockDialog
New in version NX6.0.0.
License requirements: None.
JournalPause¶
-
UI.
JournalPause
¶ Pauses execution of a journal.
Signature
JournalPause()
New in version NX4.0.0.
License requirements: None.
LockAccess¶
-
UI.
LockAccess
¶ Locks access to the NX User Interface.
This method may be used for a custom dialog that requires the session to remain in a known state. When this method is called, all menu items that would allow the user to edit the model are grayed out.
Note that until
UnlockAccess()
is called, the user will not be able to interact with the session. You must ensure that the UI is unlocked when the custom dialog terminates.This method will throw an exception if the UI cannot be locked. Note that if the UI has already been locked, then it is safe to call this method again.
Signature
LockAccess()
New in version NX3.0.0.
License requirements: None.
RemoveUtilityFunctionVisibilityHandler¶
-
UI.
RemoveUtilityFunctionVisibilityHandler
¶ Unregisters a user defined method that is called whenever an utility function state changes.
Signature
RemoveUtilityFunctionVisibilityHandler(id)
Parameters: id (int) – identifier for method to unregister New in version NX5.0.5.
License requirements: None.
UnlockAccess¶
-
UI.
UnlockAccess
¶ Unlocks access for a UI that has been locked by a call to
LockAccess()
. If the UI is already unlocked, this method has no effect.Signature
UnlockAccess()
New in version NX3.0.0.
License requirements: None.