SessionVisualizationShade Class¶
Properties¶
Property | Description |
---|---|
EdgesEmphasis | Returns or sets the edge emphasis flag. |
LwrtStudioDisplay | Returns or sets the lwrt studio display flag. |
SeeThru | Returns or sets the setting that determines whether See-Thru is applied to all less important objects. |
SeeThruDeEmphasizedObjects | Returns or sets the setting that determines whether See-Thru is applied to de-emphasized objects. |
SeeThruSection | Returns or sets the setting that determines whether See-Thru is applied to the section cap. |
SeeThruStyle | Returns or sets the see-thru style that determines how translucency is applied to less important shaded geometry. |
SeeThruStyleOptions | Returns or sets the See-Thru color, edge, and translucency options used for the various See-Thru Styles. |
ShowFacetEdges | Returns or sets the show facet edge flag. |
Methods¶
Method | Description |
---|---|
RegenerateShadedViewsFromToleranceChange | Regenerates Shaded Views. |
RegenerateStudioAnalysisViewsFromTolChange | Regenerates Studio Analysis Views. |
Enumerations¶
SessionVisualizationShadeSeeThruEdgesType Enumeration | Determines whether edges are displayed for less important shaded geometry when See-Thru is enabled. |
SessionVisualizationShadeSeeThruStyleType Enumeration | Determines how translucency is applied to less important shaded geometry when See-Thru is enabled. |
Structs¶
SessionVisualizationShadeRgb_Struct Struct | Specifies a color by its red, green, and blue values, where each value is between 0 and 1. |
SessionVisualizationShadeSeeThruOptions_Struct Struct | Specifies the See-Thru color, edge, and translucency options used for the various See-Thru Styles. |
Property Detail¶
EdgesEmphasis¶
-
SessionVisualizationShade.
EdgesEmphasis
¶ Returns or sets the edge emphasis flag.
Alters how edges are displayed when Shaded Face Edges is flag is true.
-------------------------------------
Getter Method
Signature
EdgesEmphasis()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgesEmphasis(edgesEmphasis)
Parameters: edgesEmphasis (bool) – Edge Emphasis Option to be set or not New in version NX3.0.0.
License requirements: None.
LwrtStudioDisplay¶
-
SessionVisualizationShade.
LwrtStudioDisplay
¶ Returns or sets the lwrt studio display flag.
Alters how studio are displayed.
-------------------------------------
Getter Method
Signature
LwrtStudioDisplay()
Returns: Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LwrtStudioDisplay(lwrtStudioDisplay)
Parameters: lwrtStudioDisplay (bool) – Option to be set or not New in version NX4.0.0.
License requirements: None.
SeeThru¶
-
SessionVisualizationShade.
SeeThru
¶ Returns or sets the setting that determines whether See-Thru is applied to all less important objects.
-------------------------------------
Getter Method
Signature
SeeThru()
Returns: Return type: bool New in version NX7.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.SessionVisualizationEmphasis
.License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThru(seeThru)
Parameters: seeThru (bool) – New in version NX7.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.SessionVisualizationEmphasis
.License requirements: None.
SeeThruDeEmphasizedObjects¶
-
SessionVisualizationShade.
SeeThruDeEmphasizedObjects
¶ Returns or sets the setting that determines whether See-Thru is applied to de-emphasized objects.
-------------------------------------
Getter Method
Signature
SeeThruDeEmphasizedObjects()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.SessionVisualizationEmphasis.SeeThruDeEmphasizedObjects()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruDeEmphasizedObjects(seeThruDeEmphasizedObjects)
Parameters: seeThruDeEmphasizedObjects (bool) – New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.SessionVisualizationEmphasis.SeeThruDeEmphasizedObjects()
instead.License requirements: None.
SeeThruSection¶
-
SessionVisualizationShade.
SeeThruSection
¶ Returns or sets the setting that determines whether See-Thru is applied to the section cap.
-------------------------------------
Getter Method
Signature
SeeThruSection()
Returns: Return type: bool New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.SessionVisualizationEmphasis.SeeThruSection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruSection(seeThruSection)
Parameters: seeThruSection (bool) – New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.SessionVisualizationEmphasis.SeeThruSection()
instead.License requirements: None.
SeeThruStyle¶
-
SessionVisualizationShade.
SeeThruStyle
¶ Returns or sets the see-thru style that determines how translucency is applied to less important shaded geometry.
-------------------------------------
Getter Method
Signature
SeeThruStyle()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeSeeThruStyleType
New in version NX7.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.PartVisualizationEmphasis.SeeThruStyle()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruStyle(seeThruStyle)
Parameters: seeThruStyle ( NXOpen.Preferences.SessionVisualizationShadeSeeThruStyleType
) –New in version NX7.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.PartVisualizationEmphasis.SeeThruStyle()
instead.License requirements: None.
SeeThruStyleOptions¶
-
SessionVisualizationShade.
SeeThruStyleOptions
¶ Returns or sets the See-Thru color, edge, and translucency options used for the various See-Thru Styles.
-------------------------------------
Getter Method
Signature
SeeThruStyleOptions()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeSeeThruOptions_Struct
New in version NX7.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.PartVisualizationEmphasis
.License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruStyleOptions(seeThruOptions)
Parameters: seeThruOptions ( NXOpen.Preferences.SessionVisualizationShadeSeeThruOptions_Struct
) –New in version NX7.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.PartVisualizationEmphasis
.License requirements: None.
ShowFacetEdges¶
-
SessionVisualizationShade.
ShowFacetEdges
¶ Returns or sets the show facet edge flag.
Toggles the display of facet edges. If this flag is true it can help when trying to evaluate or interpret faceted edges.
-------------------------------------
Getter Method
Signature
ShowFacetEdges()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowFacetEdges(facetEdges)
Parameters: facetEdges (bool) – New in version NX3.0.0.
License requirements: None.
Method Detail¶
RegenerateShadedViewsFromToleranceChange¶
-
SessionVisualizationShade.
RegenerateShadedViewsFromToleranceChange
¶ Regenerates Shaded Views.
Updates all objects based on their surfacing tolerance.
Signature
RegenerateShadedViewsFromToleranceChange()
New in version NX3.0.0.
License requirements: None.
RegenerateStudioAnalysisViewsFromTolChange¶
-
SessionVisualizationShade.
RegenerateStudioAnalysisViewsFromTolChange
¶ Regenerates Studio Analysis Views.
Updates all objects based on their surfacing tolerance.
Signature
RegenerateStudioAnalysisViewsFromTolChange(updateEnvOption)
Parameters: updateEnvOption (bool) – Send TRUE if env cube updation is required. Else send FALSE New in version NX3.0.0.
License requirements: None.