PartVisualizationEmphasis Class¶
-
class
NXOpen.Preferences.
PartVisualizationEmphasis
¶ Bases:
object
Represents visualization preferences for emphasis that are applicable to the entire part.
To obtain an instance of this class, refer to
NXOpen.Preferences.PartPreferences
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
EmphasisColor | Returns or sets the color applied to objects in order to emphasize them. |
SeeThruStyle | Returns or sets the See-Thru style that determines how translucency and color are used to de-emphasize shaded geometry. |
Methods¶
Method | Description |
---|---|
GetLayersOptions | Returns options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers. |
GetOriginalColorShellOptions | Returns options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. |
GetShellOptions | Returns options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell. |
GetWireframeBlendOptions | Returns options that control the color-blending effect used to de-emphasize wireframe geometry. |
SetLayersOptions | Modifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers. |
SetOriginalColorShellOptions | Modifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. |
SetShellOptions | Modifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell. |
SetWireframeBlendOptions | Modifies options that control the color-blending effect used to de-emphasize wireframe geometry. |
Enumerations¶
PartVisualizationEmphasisEdgesType Enumeration | Determines whether or not edges are displayed for de-emphasized shaded geometry. |
PartVisualizationEmphasisSeeThruStyleType Enumeration | Determines how translucency and color are used to de-emphasize shaded geometry. |
Structs¶
PartVisualizationEmphasisLayersOptions_Struct Struct | Specifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers. |
PartVisualizationEmphasisOriginalColorShellOptions_Struct Struct | Specifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. |
PartVisualizationEmphasisShellOptions_Struct Struct | Specifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell. |
PartVisualizationEmphasisWireframeBlendOptions_Struct Struct | Specifies options that control the color-blending effect used to de-emphasize wireframe geometry. |
Property Detail¶
EmphasisColor¶
-
PartVisualizationEmphasis.
EmphasisColor
¶ Returns or sets the color applied to objects in order to emphasize them.
-------------------------------------
Getter Method
Signature
EmphasisColor()
Returns: Return type: Id New in version NX8.5.0.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
EmphasisColor(emphasisColor)
Parameters: emphasisColor (Id) – New in version NX8.5.0.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: None.
SeeThruStyle¶
-
PartVisualizationEmphasis.
SeeThruStyle
¶ Returns or sets the See-Thru style that determines how translucency and color are used to de-emphasize shaded geometry.
-------------------------------------
Getter Method
Signature
SeeThruStyle()
Returns: Return type: NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruStyle(seeThruStyle)
Parameters: seeThruStyle ( NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType
) –New in version NX8.5.0.
License requirements: None.
Method Detail¶
GetLayersOptions¶
-
PartVisualizationEmphasis.
GetLayersOptions
¶ Returns options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers.
Signature
GetLayersOptions()
Returns: options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers. :rtype:
NXOpen.Preferences.PartVisualizationEmphasisLayersOptions_Struct
New in version NX8.5.0.
License requirements: None.
GetOriginalColorShellOptions¶
-
PartVisualizationEmphasis.
GetOriginalColorShellOptions
¶ Returns options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.
Signature
GetOriginalColorShellOptions()
Returns: options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. :rtype:
NXOpen.Preferences.PartVisualizationEmphasisOriginalColorShellOptions_Struct
New in version NX8.5.0.
License requirements: None.
GetShellOptions¶
-
PartVisualizationEmphasis.
GetShellOptions
¶ Returns options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell.
Signature
GetShellOptions()
Returns: options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell. :rtype:
NXOpen.Preferences.PartVisualizationEmphasisShellOptions_Struct
New in version NX8.5.0.
License requirements: None.
GetWireframeBlendOptions¶
-
PartVisualizationEmphasis.
GetWireframeBlendOptions
¶ Returns options that control the color-blending effect used to de-emphasize wireframe geometry.
Signature
GetWireframeBlendOptions()
Returns: options that control the color-blending effect used to de-emphasize wireframe geometry. :rtype:
NXOpen.Preferences.PartVisualizationEmphasisWireframeBlendOptions_Struct
New in version NX8.5.0.
License requirements: None.
SetLayersOptions¶
-
PartVisualizationEmphasis.
SetLayersOptions
¶ Modifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers.
Signature
SetLayersOptions(layersOptions)
Parameters: layersOptions ( NXOpen.Preferences.PartVisualizationEmphasisLayersOptions_Struct
) – options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Layers.New in version NX8.5.0.
License requirements: None.
SetOriginalColorShellOptions¶
-
PartVisualizationEmphasis.
SetOriginalColorShellOptions
¶ Modifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.
Signature
SetOriginalColorShellOptions(originalColorShellOptions)
Parameters: originalColorShellOptions ( NXOpen.Preferences.PartVisualizationEmphasisOriginalColorShellOptions_Struct
) – options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.New in version NX8.5.0.
License requirements: None.
SetShellOptions¶
-
PartVisualizationEmphasis.
SetShellOptions
¶ Modifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell.
Signature
SetShellOptions(shellOptions)
Parameters: shellOptions ( NXOpen.Preferences.PartVisualizationEmphasisShellOptions_Struct
) – options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Shell.New in version NX8.5.0.
License requirements: None.
SetWireframeBlendOptions¶
-
PartVisualizationEmphasis.
SetWireframeBlendOptions
¶ Modifies options that control the color-blending effect used to de-emphasize wireframe geometry.
Signature
SetWireframeBlendOptions(wireframeBlendOptions)
Parameters: wireframeBlendOptions ( NXOpen.Preferences.PartVisualizationEmphasisWireframeBlendOptions_Struct
) – options that control the color-blending effect used to de-emphasize wireframe geometry.New in version NX8.5.0.
License requirements: None.