PartVisualizationEmphasisEdgesType Enumeration

NXOpen.Preferences.PartVisualizationEmphasis.EdgesType is an alias for NXOpen.Preferences.PartVisualizationEmphasisEdgesType

class NXOpen.Preferences.PartVisualizationEmphasisEdgesType

Bases: object

Determines whether or not edges are displayed for de-emphasized shaded geometry.

Enum Members

Displays no edges for de-emphasized shaded geometry. “
“Normal”, “

Displays edges for de-emphasized shaded geometry if edges are normally displayed for shaded geometry. “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.