PartVisualizationEmphasisSeeThruStyleType Enumeration

NXOpen.Preferences.PartVisualizationEmphasis.SeeThruStyleType is an alias for NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType

class NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType

Bases: object

Determines how translucency and color are used to de-emphasize shaded geometry.

Enum Members

Displays de-emphasized shaded geometry as a translucent shell with a single color. “

“OriginalColorShell”, “

Displays de-emphasized shaded geometry as a translucent shell, preserving original colors. “

“Layers”, “

Displays de-emphasized shaded geometry as translucent layers with a single color. “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.