SessionVisualizationShadeSeeThruStyleType Enumeration

NXOpen.Preferences.SessionVisualizationShade.SeeThruStyleType is an alias for NXOpen.Preferences.SessionVisualizationShadeSeeThruStyleType

class NXOpen.Preferences.SessionVisualizationShadeSeeThruStyleType

Bases: object

Determines how translucency is applied to less important shaded geometry when See-Thru is enabled.

Deprecated since version NX8.5.0: Use NXOpen.Preferences.PartVisualizationEmphasisSeeThruStyleType instead.

Enum Members

Displays less important shaded geometry as a translucent shell with a specified color. “

“OriginalColorShell”, “

Displays less important shaded geometry as a translucent shell, preserving original shaded geometry colors. “

“Layers”, “

Displays less important shaded geometry as translucent layers with a specified color. “

ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.