SessionVisualizationShadeSeeThruEdgesType Enumeration¶
NXOpen.Preferences.SessionVisualizationShade.SeeThruEdgesType is an alias for NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
-
class
NXOpen.Preferences.
SessionVisualizationShadeSeeThruEdgesType
¶ Bases:
object
Determines whether edges are displayed for less important shaded geometry when See-Thru is enabled.
Deprecated since version NX8.5.0: Use
NXOpen.Preferences.PartVisualizationEmphasisEdgesType
instead.Enum Members
- Displays no edges for less important shaded geometry. “
- “Normal”, “
Displays edges for less important shaded geometry if edges are normally displayed for shaded geometry. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.