SessionVisualizationVisual Class

class NXOpen.Preferences.SessionVisualizationVisual

Bases: object

Represents all UI based session Visualization visual preferences

To obtain an instance of this class, refer to NXOpen.UI

New in version NX3.0.0.

Properties

Property Description
FullSceneAntialiasing Returns or sets the scene antialiasing flag.
LineAntialiasing Returns or sets the line antialiasing flag.
Translucency Returns or sets the translucency flag.

Methods

Property Detail

FullSceneAntialiasing

SessionVisualizationVisual.FullSceneAntialiasing

Returns or sets the scene antialiasing flag.

-------------------------------------

Getter Method

Signature FullSceneAntialiasing()

Returns:
Return type:bool

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FullSceneAntialiasing(fullSceneAntialiasing)

Parameters:fullSceneAntialiasing (bool) –

New in version NX3.0.0.

License requirements: None.

LineAntialiasing

SessionVisualizationVisual.LineAntialiasing

Returns or sets the line antialiasing flag.

True value specifies that lines, curves, and edges are drawn more smoothly

-------------------------------------

Getter Method

Signature LineAntialiasing()

Returns:
Return type:bool

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LineAntialiasing(lineAntialiasing)

Parameters:lineAntialiasing (bool) –

New in version NX3.0.0.

License requirements: None.

Translucency

SessionVisualizationVisual.Translucency

Returns or sets the translucency flag.

True value specifies that each shaded object is drawn with the translucency setting specified with Edit-<ja_gt>Object Display. False value specify that all objects in Fully Shaded or Partially Shaded views appear opaque, regardless of their individual translucency settings.

-------------------------------------

Getter Method

Signature Translucency()

Returns:
Return type:bool

New in version NX3.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Translucency(translucency)

Parameters:translucency (bool) –

New in version NX3.0.0.

License requirements: None.