MovieManager Class¶
-
class
NXOpen.
MovieManager
¶ Bases:
object
Represents a
MovieManager
class. This class is used for recording movies.To obtain an instance of this class, refer to
NXOpen.UI
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CaptureFrame | Use this method to capture a frame at a specified point. |
CreateMovieSettingsBuilder | Creates a MovieSettingsBuilder @return |
End | Stops movie recording |
Pause | Pauses movie recording |
Resume | Resumes movie recording |
SetPlaybackSpeed | Sets the movie playback speed. |
Start | Starts movie recording |
Method Detail¶
CaptureFrame¶
-
MovieManager.
CaptureFrame
¶ Use this method to capture a frame at a specified point.
This is used when the movie recording was started with true as the second parameter of
MovieManager.Start()
Signature
CaptureFrame()
New in version NX6.0.0.
License requirements: None.
CreateMovieSettingsBuilder¶
-
MovieManager.
CreateMovieSettingsBuilder
¶ Creates a
MovieSettingsBuilder
Signature
CreateMovieSettingsBuilder()
Returns: Return type: NXOpen.MovieSettingsBuilder
New in version NX6.0.0.
License requirements: None.
End¶
-
MovieManager.
End
¶ Stops movie recording
Signature
End()
New in version NX6.0.0.
License requirements: None.
Pause¶
-
MovieManager.
Pause
¶ Pauses movie recording
Signature
Pause()
New in version NX6.0.0.
License requirements: None.
Resume¶
-
MovieManager.
Resume
¶ Resumes movie recording
Signature
Resume()
New in version NX6.0.0.
License requirements: None.
SetPlaybackSpeed¶
-
MovieManager.
SetPlaybackSpeed
¶ Sets the movie playback speed.
Movie may not play appropriately at a very high rate (few hundreds). In such cases a lower value could be set. Recommendation is to use a value less than 100 fps.
Signature
SetPlaybackSpeed(fps)
Parameters: fps (int) – Specifies the playback speed of the movie in frames per second. New in version NX8.0.0.
License requirements: None.
Start¶
-
MovieManager.
Start
¶ Starts movie recording
Signature
Start(filename, userFrames)
Parameters: - filename (str) – Filename of the movie to be createed
- userFrames (bool) – If true, user will provide frames through
MovieManager.CaptureFrame()
. If false, system generates frames
New in version NX6.0.0.
License requirements: None.