VisualizationLine Class¶
Properties¶
Property | Description |
---|---|
DepthSortedWireframe | Returns or sets the depth sorted wireframe. |
WireframeContrast | Returns or sets whether colors applied to wireframe geometry are automatically adjusted as necessary to produce a minimum contrast relative to the view background. |
Methods¶
Method | Description |
---|---|
RegenerateFromToleranceChange | Regenerates after changing tolerance |
UpdateLineFontObjects | Updates the UI after line font is changed |
Property Detail¶
DepthSortedWireframe¶
-
VisualizationLine.
DepthSortedWireframe
¶ Returns or sets the depth sorted wireframe.
Specifies whether the graphics driver should sort objects by depth in wireframe views.
-------------------------------------
Getter Method
Signature
DepthSortedWireframe()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthSortedWireframe(depthSortedWireframe)
Parameters: depthSortedWireframe (bool) – New in version NX3.0.0.
License requirements: None.
WireframeContrast¶
-
VisualizationLine.
WireframeContrast
¶ Returns or sets whether colors applied to wireframe geometry are automatically adjusted as necessary to produce a minimum contrast relative to the view background.
The option affects onscreen displays only, so it affects interactive displays and raster images captured from interactive displays. It does not affect vector output produced by Plot, Print, CGM Export and similar functions.
-------------------------------------
Getter Method
Signature
WireframeContrast()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WireframeContrast(wireframeContrast)
Parameters: wireframeContrast (bool) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
RegenerateFromToleranceChange¶
-
VisualizationLine.
RegenerateFromToleranceChange
¶ Regenerates after changing tolerance
Signature
RegenerateFromToleranceChange(updateModeChange, studio)
Parameters: - updateModeChange (bool) – whether update_mode has changed
- studio (bool) – studio or non studio
New in version NX3.0.0.
License requirements: None.
UpdateLineFontObjects¶
-
VisualizationLine.
UpdateLineFontObjects
¶ Updates the UI after line font is changed
Signature
UpdateLineFontObjects(doSoftwareUpdate)
Parameters: doSoftwareUpdate (bool) – The do_software_update flag should be set to TRUE when changing from software fonts to hardware fonts or when changing dash New in version NX3.0.0.
License requirements: None.