PreviewPropertiesBuilderModelViewCreationOptions Enumeration¶
NXOpen.PreviewPropertiesBuilder.ModelViewCreationOptions is an alias for NXOpen.PreviewPropertiesBuilderModelViewCreationOptions
-
class
NXOpen.
PreviewPropertiesBuilderModelViewCreationOptions
¶ Bases:
object
Specifies when the model view preview will be created
Enum Members
Enum Member Enum Member Description OnPartSave Model view preview will be created when the part is savedOnViewSave Model view preview will be created when the view is savedOnDemand Interactive only option that allows the model view preview to be created by selected the Create Now button-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-