EdgeTangentRule Class¶
-
class
NXOpen.
EdgeTangentRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects tangent connected edges from the body of the seed edge.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge tangent rule: NXOpen.EdgeTangentRule |
Method Detail¶
Dispose¶
-
EdgeTangentRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeTangentRule.
GetData
¶ Gets the data for the edge tangent rule:
NXOpen.EdgeTangentRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (startEdge, endEdge, isFromStart, angleTolerance, hasSameConvexity). startEdge is a
NXOpen.Edge
. Start edge of edge tangent ruleendEdge is aNXOpen.Edge
. End edge of edge tangent rule. It can be null (Nothing).isFromStart is a bool. True: the tangent starts from the start point of the start edge if end edge is providedangleTolerance is a float. Angle tolerance for tangent edges hasSameConvexity is a bool. True: will only find tangnet edges that has the same convexity .. versionadded:: NX3.0.0License requirements: gateway (“UG GATEWAY”)