SelectionIntentRule Class¶
-
class
NXOpen.
SelectionIntentRule
¶ Bases:
NXOpen.TransientObject
Represents a
NXOpen.SelectionIntentRule
which essentially provides capabilities to collect curves, edges, faces and bodies.The intent of the collection is remembered as a rule in the corresponding
NXOpen.Section
orNXOpen.ScCollector
.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Enumerations¶
SelectionIntentRuleRuleType Enumeration | This enum represents the type of selection intent rules as specified by NXOpen.SelectionIntentRule |
Property Detail¶
Type¶
-
SelectionIntentRule.
Type
¶ Returns the get the type of selection intent rule:
NXOpen.SelectionIntentRule
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.SelectionIntentRuleRuleType
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
Method Detail¶
Dispose¶
-
SelectionIntentRule.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.