Section Class¶
-
class
NXOpen.
Section
¶ Bases:
NXOpen.DisplayableObject
Represents a section
Section consists of “chained_entity”, a chain or a single entity of edge or curve. The entire chain(or a single entity) may be used by the section or only a portion of the chain (or single entity) might be used. The portion of the chain (or single entity) that is used is defined by the “start_connector” and “end_connector”.
start_connector: It represents the start of the portion of the chain (or single entity) that is used. If “start_connector” is null (Nothing), then the start point of the chained_entity along its “natural” direction is used.
start_connector_intersection_point: The point of intersection of the “chained_entity” and the “start_connector”. This is used to determine what portion of the chain to use in case the “start_connector” intersects the “chained_entity” in multiple locations.
end_connector: It represents the end of the portion of the chain (or single entity) that is used.
end_connector_intersection_point: The point of intersection of the “chained_entity” and the “end_connector”. This is used to determine what portion of the chain to use in case the “end_connector” intersects the “chained_entity” in multiple locations.
To create a new instance of this class, use
NXOpen.SectionCollection.CreateSection()
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
ChainingTolerance | Returns or sets the chaining tolerance |
Color | Returns or sets the color of the object. |
DistanceTolerance | Returns or sets the distance tolerance |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddChainBetweenIntersectionPoints | Adds a chain between given two intersection points to the section. |
AddSmartPoint | Add smart point into section. |
AddToSection | Adds selection intent rules to the section. |
AlignDirectionOfLoop | Set the direction of a single loop of the section along the given vector. |
AllowSelfIntersection | Allow self intersecting section or not. |
Blank | Blanks the object. |
CleanMappingData | Cleans Mapping Data |
Clear | Clear the section of all its constituents |
CloneSection | Clone section. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DeselectPortion | Deselects Portion of the section depending on the option provided. |
Destroy | Destroy the section object |
EvaluateAndAskOutputEntities | Recalculates section collection. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllowedEntityTypes | Get the Allowed Entity Types. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLoopIndex | Returns the index of the section loop conatining the section element. |
GetMultiComponent | Gets the option set on Section for collection from multiple components. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNonFeatureMode | Gets the option set on Section for collection in non-feature mode. |
GetOldOutputCurves | Gives the old output curves of the section. |
GetOutputCurves | Gives the output curves of the section. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSectionData | Gets the section data |
GetStartAndDirection | Gets the start element and the direction of the section. |
GetStartAndDirectionOfLoop | Gets the start point and the direction of a specified single loop of the section. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Highlight | Highlights the object. |
MapSectionElements | Maps old section curves to new section curves |
PrepareMappingData | Prepares Mapping Data |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveMultipleCurves | Removes multiple section elements that are either curves/edges. |
RemoveMultipleElements | Removes multiple section elements. |
RemoveMultiplePoints | Removes multiple section elements that are points. |
RemoveRules | Removes selection intent rules from the section. |
RemoveSingleSectionElement | Removes one section element curve. |
RemoveUnderlyingChain | Removes all the selection intent rules related to the chain on which the given point lies. |
RemoveUnderlyingCurve | Removes the single curve which is within tolerance to the given point, from the section. |
RemoveViewDependency | Remove dependency on all views from an object. |
ReverseDirection | Reverse the section direction |
ReverseDirectionOfClosedLoop | Reverse the loop direction of a closed loop while keeping the start curve same. |
ReverseDirectionOfLoop | Reverse the direction of of a specified single loop of the section. |
SetAllowRefCrvs | Sets to the section whether to allow reference curves or not. |
SetAllowedEntityTypes | Set the Allowed Entity Types. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetInterpart | Set inter-part state of section and make it empty. |
SetMultiComponent | Sets the true option on Section for collection from multiple components. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetNonFeatureMode | Sets the true option on Section for collection in non-feature mode. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetStartAndDirection | Sets the start element and the direction of the section. |
SetStartCurveOfClosedLoop | Set the curve on which the specified point lies as the start curve of a specified single loop of the section. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SkipSorting | Sets the option to skip sorting the section loops or not. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
SectionAllowTypes Enumeration | Defines entity types allowed. |
SectionDeselectOption Enumeration | Defines type of deselect option. |
SectionMode Enumeration | Defines mode with respect to feature create or edit mode. |
Property Detail¶
AngleTolerance¶
-
Section.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: angle tolerance Return type: float New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – angle tolerance New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
ChainingTolerance¶
-
Section.
ChainingTolerance
¶ Returns or sets the chaining tolerance
-------------------------------------
Getter Method
Signature
ChainingTolerance()
Returns: chaining tolerance Return type: float New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Setter Method
Signature
ChainingTolerance(chainingTolerance)
Parameters: chainingTolerance (float) – chaining tolerance New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
DistanceTolerance¶
-
Section.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: distance tolerance Return type: float New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – distance tolerance New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
IsOccurrence¶
-
Section.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Section.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Section.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Section.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Section.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Section.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddChainBetweenIntersectionPoints¶
-
Section.
AddChainBetweenIntersectionPoints
¶ Adds a chain between given two intersection points to the section.
Signature
AddChainBetweenIntersectionPoints(rules, startConnector, startIntersectionPoint, endConnector, endIntersectionPoint, seed, helpPoint, featureMode, chainWithinFeature)
Parameters: - rules (list of
NXOpen.SelectionIntentRule
) – Selection intent rules. To create selection intent rules see documentation ofScRuleFactory
for more details. - startConnector (
NXOpen.NXObject
) – It represents the start of the portion of the chain (or single entity) that is used. If “startConnector” is None, then the start point of the chained entity along its “natural” direction is used. It can be point, curve or edge - startIntersectionPoint (
NXOpen.Point3d
) – The point where the start connector intersects with the chain. - endConnector (
NXOpen.NXObject
) – Represents the end of the portion of the chain (or single entity) that is used. It can be point, curve or edge - endIntersectionPoint (
NXOpen.Point3d
) – The point where the end connector intersects with the chain. - seed (
NXOpen.NXObject
) – Seed curve, edge or face - helpPoint (
NXOpen.Point3d
) – The point which is used to determine which portion of the chain to use for creating section. - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode. - chainWithinFeature (bool) – True if chaining and discovery of intersection limits is to be restricted to the feature of the seed. This is effective only when the seed belongs to a curve feature.
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
- rules (list of
AddSmartPoint¶
-
Section.
AddSmartPoint
¶ Add smart point into section.
This API is now deprecated. Please use
ScRuleFactory.CreateRuleCurveDumb()
andSection.AddToSection()
instead.Signature
AddSmartPoint(smartPt, tol)
Parameters: - smartPt (
NXOpen.Point
) – Smart point tobe added into section. - tol (float) – Tolerance.
New in version NX4.0.0.
Deprecated since version NX7.5.0: Please use
ScRuleFactory.CreateRuleCurveDumb()
followed bySection.AddToSection()
instead.License requirements: gateway (“UG GATEWAY”)
- smartPt (
AddToSection¶
-
Section.
AddToSection
¶ Overloaded method AddToSection
AddToSection(rules, seed, startConnector, endConnector, helpPoint, featureMode)
AddToSection(rules, seed, startConnector, endConnector, helpPoint, featureMode, chainWithinFeature)
-------------------------------------
Adds selection intent rules to the section.
Signature
AddToSection(rules, seed, startConnector, endConnector, helpPoint, featureMode)
Parameters: - rules (list of
NXOpen.SelectionIntentRule
) – Selection intent rules. To create selection intent rules see documentation ofScRuleFactory
for more details. - seed (
NXOpen.NXObject
) – Seed curve, edge or face - startConnector (
NXOpen.NXObject
) – It represents the start of the portion of the chain (or single entity) that is used. If “start_connector” is null (Nothing), then the start point of the chained_entity along its “natural” direction is used. It can be point, curve or edge - endConnector (
NXOpen.NXObject
) – It represents the end of the portion of the chain (or single entity) that is used. It can be point, curve or edge - helpPoint (
NXOpen.Point3d
) – When ambiguity in multiple solutions is encountered, help_point is used to determine which portion of the chain to use for creating section. It is most useful when used with non-NULL connectors or with Region Boundary Curves rule. - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Adds selection intent rules to the section with the option of restricting chaining and limit discovery to a single feature.
Signature
AddToSection(rules, seed, startConnector, endConnector, helpPoint, featureMode, chainWithinFeature)
Parameters: - rules (list of
NXOpen.SelectionIntentRule
) – Selection intent rules. To create selection intent rules see documentation ofScRuleFactory
for more details. - seed (
NXOpen.NXObject
) – Seed curve, edge or face - startConnector (
NXOpen.NXObject
) – It represents the start of the portion of the chain (or single entity) that is used. If “start_connector” is null (Nothing), then the start point of the chained_entity along its “natural” direction is used. It can be point, curve or edge - endConnector (
NXOpen.NXObject
) – It represents the end of the portion of the chain (or single entity) that is used. It can be point, curve or edge - helpPoint (
NXOpen.Point3d
) – When ambiguity in multiple solutions is encountered, help_point is used to determine which portion of the chain to use for creating section. It is most useful when used with non-NULL connectors or with Region Boundary Curves rule. - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode. - chainWithinFeature (bool) – True if chaining and discovery of intersection limits is to be restricted to the feature of the seed. This is effective only when the seed belongs to a curve feature.
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
AlignDirectionOfLoop¶
-
Section.
AlignDirectionOfLoop
¶ Set the direction of a single loop of the section along the given vector.
Signature
AlignDirectionOfLoop(point, direction)
Parameters: - point (
NXOpen.Point3d
) – Any point on a the desired loop. - direction (
NXOpen.Vector3d
) – Desired tangent direction of the loop at the point.
New in version NX5.0.1.
License requirements: gateway (“UG GATEWAY”)
- point (
AllowSelfIntersection¶
-
Section.
AllowSelfIntersection
¶ Allow self intersecting section or not.
By default self intersection is allowed.
Signature
AllowSelfIntersection(allowSelfIntersection)
Parameters: allowSelfIntersection (bool) – True if self-intersecting section is allowed else false New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
CleanMappingData¶
-
Section.
CleanMappingData
¶ Cleans Mapping Data
This method should be used to clean mapping data after mapping is done
Signature
CleanMappingData()
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
Clear¶
-
Section.
Clear
¶ Clear the section of all its constituents
Signature
Clear()
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
CloneSection¶
-
Section.
CloneSection
¶ Clone section.
Signature
CloneSection()
Returns: the cloned section Return type: NXOpen.Section
New in version NX7.0.0.
License requirements: None.
DeselectPortion¶
-
Section.
DeselectPortion
¶ Deselects Portion of the section depending on the option provided.
This method should be used to deselect portion of the section.
Signature
DeselectPortion(seedPoint, startLimit, endLimit, deselectionType)
Parameters: - seedPoint (
NXOpen.Point3d
) – The seed point of deselection - startLimit (
NXOpen.NXObject
) – The element that is connected to the curve/edge near its start point. - endLimit (
NXOpen.NXObject
) – The element that is connected to the curve/edge near its end point. - deselectionType (
NXOpen.SectionDeselectOption
) – The deselection type
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
- seedPoint (
Destroy¶
-
Section.
Destroy
¶ Destroy the section object
Signature
Destroy()
New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
EvaluateAndAskOutputEntities¶
-
Section.
EvaluateAndAskOutputEntities
¶ Recalculates section collection.
This is JA API for recalculating the section collection and to get the section collection after recalculation.
Signature
EvaluateAndAskOutputEntities()
Returns: The array of section elements. Return type: list of NXOpen.NXObject
New in version NX9.0.0.
License requirements: gateway (“UG GATEWAY”)
FindObject¶
-
Section.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAllowedEntityTypes¶
-
Section.
GetAllowedEntityTypes
¶ Get the Allowed Entity Types.
Works only for UF_SC_CURVE_dumb_data_s and UF_SC_CURVE_feature_data_s
Signature
GetAllowedEntityTypes()
Returns: allowed entity types Return type: NXOpen.SectionAllowTypes
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
GetLoopIndex¶
-
Section.
GetLoopIndex
¶ Overloaded method GetLoopIndex
GetLoopIndex(sectionElement)
GetLoopIndex(pointSpecifyingLoop, tolerance)
-------------------------------------
Returns the index of the section loop conatining the section element. If the section element does not exist in the section or is part of more than one loops, this method will return an error.
Signature
GetLoopIndex(sectionElement)
Parameters: sectionElement ( NXOpen.NXObject
) – an element that constructs the sectionReturns: loop Index Return type: int New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Returns the index of the loop on which the given point lies.
Signature
GetLoopIndex(pointSpecifyingLoop, tolerance)
Parameters: - pointSpecifyingLoop (
NXOpen.Point3d
) – a point lying on the loop for which the loop index is being queried - tolerance (float) – Tolerance for specifying point on loop.
Returns: loop Index
Return type: int
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
GetMultiComponent¶
-
Section.
GetMultiComponent
¶ Gets the option set on Section for collection from multiple components.
A multi-component Section can have collection from multiple components i.e., multiple parts or multiple instances of same part or both.
Signature
GetMultiComponent()
Returns: Multi-component option set on Section Return type: bool New in version NX9.0.0.
License requirements: None.
GetNonFeatureMode¶
-
Section.
GetNonFeatureMode
¶ Gets the option set on Section for collection in non-feature mode.
A Section in non-feature mode does not reference the feature data of the part from which the collection is done.
Signature
GetNonFeatureMode()
Returns: Non-feature mode set on Section Return type: bool New in version NX9.0.0.
License requirements: None.
GetOldOutputCurves¶
-
Section.
GetOldOutputCurves
¶ Gives the old output curves of the section.
This method returns an array of old section curves. They were created internally and are different from the parent curves used to build the section. These curves should not be modified or deleted, doing so may result in part corruption and session may become unstable.
Signature
GetOldOutputCurves()
Returns: The array of old section elements. Return type: list of NXOpen.NXObject
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
GetOutputCurves¶
-
Section.
GetOutputCurves
¶ Gives the output curves of the section.
This method returns an array of existing section curves. They are created internally and are different from the parent curves used to build the section. These curves should not be modified or deleted, doing so may result in part corruption and session may become unstable.
Signature
GetOutputCurves()
Returns: The array of section elements. Return type: list of NXOpen.NXObject
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
GetSectionData¶
-
Section.
GetSectionData
¶ Gets the section data
Signature
GetSectionData()
Returns: Section data consists of selection intent rules, section elements, start and end connector. :rtype: list of
NXOpen.SectionData
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
GetStartAndDirection¶
-
Section.
GetStartAndDirection
¶ Gets the start element and the direction of the section.
Signature
GetStartAndDirection()
Returns: a tuple Return type: A tuple consisting of (startElement, startPoint, direction). startElement is a NXOpen.ICurve
. The element, curve or edge, specifying the starting of the section. If start element is point then this function will return error. If the section is a loop, then the loop is started by start_element and the direction is followed the input direction. If the section is not a loop, then the section can be started by other element, but the direction of the section is defined by the start_element and direction. startPoint is aNXOpen.Point3d
. The origin of the vector that defines the direction of the section. This point has to be on the start_element. direction is aNXOpen.Vector3d
. The direction of the vector defines the direction of the section.New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
GetStartAndDirectionOfLoop¶
-
Section.
GetStartAndDirectionOfLoop
¶ Gets the start point and the direction of a specified single loop of the section.
Signature
GetStartAndDirectionOfLoop(index)
Parameters: index (int) – The index of the loop of the section for which start point and direction are being queried. Returns: a tuple Return type: A tuple consisting of (startPoint, direction). startPoint is a NXOpen.Point3d
. The origin of the vector that defines the direction of the loop of the section specified by the index. direction is aNXOpen.Vector3d
. The direction of the vector defines the direction of the loop of the section specified by the index.New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
MapSectionElements¶
-
Section.
MapSectionElements
¶ Maps old section curves to new section curves
This method should be used to map old section curves to new section curves when some or all curves from section are removed and some or all new curves are added.
To find old section curves see documentation for
Section.GetOldOutputCurves()
and to find current section curves see documentation forSection.GetOutputCurves()
Signature
MapSectionElements(oldWf, newWf)
Parameters: - oldWf (
NXOpen.NXObject
) – The old section curve which was removed and hence needs to be mapped. - newWf (
NXOpen.NXObject
) – The new section curve that would be mapped to the old section curve.
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
- oldWf (
PrepareMappingData¶
-
Section.
PrepareMappingData
¶ Prepares Mapping Data
This method should be used to create mapping data if mapping is to be done
Signature
PrepareMappingData()
New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
Print¶
-
Section.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveMultipleCurves¶
-
Section.
RemoveMultipleCurves
¶ Removes multiple section elements that are either curves/edges.
This API is now deprecated. Please use
Section.RemoveMultipleElements()
instead.Signature
RemoveMultipleCurves(wfs, startConnector, endConnector, featureMode)
Parameters: - wfs (list of
NXOpen.ICurve
) – The elements (curves/edges) that construct the section. - startConnector (list of
NXOpen.NXObject
) – The element that is connected to the curve/edge near its start point. - endConnector (list of
NXOpen.NXObject
) – The element that is connected to the curve/edge near its end point. - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX6.0.2.
Deprecated since version NX8.5.0: Please use
Section.RemoveMultipleElements()
instead.License requirements: None.
- wfs (list of
RemoveMultipleElements¶
-
Section.
RemoveMultipleElements
¶ Removes multiple section elements.
This method should be used to remove the multiple section elements from section when elements to be removed contains points, and some or all curves that can not be uniquely mapped with wireframe , start connector and end connector. For Such curves point laying on the curve should be specified
Signature
RemoveMultipleElements(wfs, startConnectors, endConnectors, isCombinationsResultIntoOnlyOneCurvePerCombination, pointsOnCurvesToBeRemoved, points, featureMode)
Parameters: - wfs (list of
NXOpen.ICurve
) – The elements (curves/edges) that construct the section. - startConnectors (list of
NXOpen.NXObject
) – The element that is connected to the curve/edge near its start point. - endConnectors (list of
NXOpen.NXObject
) – The element that is connected to the curve/edge near its end point. - isCombinationsResultIntoOnlyOneCurvePerCombination (list of bool) – Whether the combination of input curve/edge, Start Connector end Connector produces unique combination (i.e. they map to single section element) or not.
- pointsOnCurvesToBeRemoved (list of
NXOpen.Point3d
) – If Combination can not define curve to be deselected uniquely, then point which lies on the curve to be removed should be provided, otherwise point must be given as (0, 0, 0) for corresponding combination - points (list of
NXOpen.Point
) – The points that are part of section and to be removed from the section. - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX6.0.2.
License requirements: gateway (“UG GATEWAY”)
- wfs (list of
RemoveMultiplePoints¶
-
Section.
RemoveMultiplePoints
¶ Removes multiple section elements that are points.
This API is now deprecated. Please use
Section.RemoveMultipleElements()
instead.Signature
RemoveMultiplePoints(points, featureMode)
Parameters: - points (list of
NXOpen.Point
) – The points that construct the section. - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX6.0.2.
Deprecated since version NX8.5.0: Please use
Section.RemoveMultipleElements()
instead.License requirements: gateway (“UG GATEWAY”)
- points (list of
RemoveRules¶
-
Section.
RemoveRules
¶ Overloaded method RemoveRules
RemoveRules(rules, startConnector, endConnector, featureMode)
RemoveRules(sectionElement, startConnector, endConnector, featureMode)
-------------------------------------
Removes selection intent rules from the section.
To get selection intent rules of the section see documentation for
Section.GetSectionData()
andSectionData.GetRules()
for more details.Signature
RemoveRules(rules, startConnector, endConnector, featureMode)
Parameters: - rules (list of
NXOpen.SelectionIntentRule
) – Selection intent rules. - startConnector (
NXOpen.NXObject
) – It represents the start of the portion of the chain (or single entity) that is used. If “start_connector” is null (Nothing), then the start point of the chained_entity along its “natural” direction is used. It can be be point, curve or edge - endConnector (
NXOpen.NXObject
) – It represents the end of the portion of the chain (or single entity) that is used. It can be be point, curve or edge - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Removes all the selection intent rules related to the section element.
To get selection elements of the section, see documentation for
Section.GetSectionData()
andSectionData.GetSectionElementsData()
for more details.Signature
RemoveRules(sectionElement, startConnector, endConnector, featureMode)
Parameters: - sectionElement (
NXOpen.ICurve
) – The element that constructs the section - startConnector (
NXOpen.NXObject
) – The element that is connected to the section_element near its start_point - endConnector (
NXOpen.NXObject
) – The element that is connected to the section_element near its end_point - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
RemoveSingleSectionElement¶
-
Section.
RemoveSingleSectionElement
¶ Overloaded method RemoveSingleSectionElement
RemoveSingleSectionElement(sectionElement, startConnector, endConnector, featureMode)
RemoveSingleSectionElement(sectionElement, featureMode)
-------------------------------------
Removes one section element curve.
To get selection element see documentation for
Section.GetSectionData()
andSectionData.GetSectionElementsData()
for more details.Signature
RemoveSingleSectionElement(sectionElement, startConnector, endConnector, featureMode)
Parameters: - sectionElement (
NXOpen.ICurve
) – The element that constructs the section - startConnector (
NXOpen.NXObject
) – The element that is connected to the section_element near its start_point - endConnector (
NXOpen.NXObject
) – The element that is connected to the section_element near its end_point - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode
New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Removes one section element that is a point.
To get selection element see documentation for
Section.GetSectionData()
andSectionData.GetSectionElementsData()
for more details.Signature
RemoveSingleSectionElement(sectionElement, featureMode)
Parameters: - sectionElement (
NXOpen.Point
) – The point that constructs the section - featureMode (
NXOpen.SectionMode
) – Feature create or edit mode
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
RemoveUnderlyingChain¶
-
Section.
RemoveUnderlyingChain
¶ Removes all the selection intent rules related to the chain on which the given point lies.
This method should be used in place of
Section.RemoveRules()
when the part containing the section element is not loaded.Signature
RemoveUnderlyingChain(pointSpecifyingChain, tolerance, featureMode)
Parameters: - pointSpecifyingChain (
NXOpen.Point3d
) – The point should lie on the chain that is to be removed. - tolerance (float) – Tolerance for specifying point on chain.
- featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
- pointSpecifyingChain (
RemoveUnderlyingCurve¶
-
Section.
RemoveUnderlyingCurve
¶ Removes the single curve which is within tolerance to the given point, from the section.
This method should be used in place of
Section.RemoveSingleSectionElement()
in any of the conditions: when the part containing the section element is not loaded, when the combination of input curve, start connector and end connector maps to multiple section element, or when underlying parent is invalid.Signature
RemoveUnderlyingCurve(pointSpecifyingCurve, tolerance, featureMode)
Parameters: - pointSpecifyingCurve (
NXOpen.Point3d
) – The point should lie on the curve that is to be removed. - tolerance (float) – Tolerance for specifying point on curve.
- featureMode (
NXOpen.SectionMode
) – Feature create or edit mode.
New in version NX6.0.2.
License requirements: gateway (“UG GATEWAY”)
- pointSpecifyingCurve (
ReverseDirection¶
-
Section.
ReverseDirection
¶ Reverse the section direction
Signature
ReverseDirection()
New in version NX4.0.0.
License requirements: gateway (“UG GATEWAY”)
ReverseDirectionOfClosedLoop¶
-
Section.
ReverseDirectionOfClosedLoop
¶ Reverse the loop direction of a closed loop while keeping the start curve same.
This API can only be used closed loops.
Signature
ReverseDirectionOfClosedLoop(index)
Parameters: index (int) – Index of the closed loop for which the direction is to be reversed. New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
ReverseDirectionOfLoop¶
-
Section.
ReverseDirectionOfLoop
¶ Reverse the direction of of a specified single loop of the section.
Signature
ReverseDirectionOfLoop(index)
Parameters: index (int) – The index of the loop of the section that is to be reversed. New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
SetAllowRefCrvs¶
-
Section.
SetAllowRefCrvs
¶ Sets to the section whether to allow reference curves or not.
This is JA API for setting to the section whether to allow reference curves or not.
Signature
SetAllowRefCrvs(allowRefCrvs)
Parameters: allowRefCrvs (bool) – New in version NX10.0.0.
License requirements: None.
SetAllowedEntityTypes¶
-
Section.
SetAllowedEntityTypes
¶ Set the Allowed Entity Types.
Works only for UF_SC_CURVE_dumb_data_s and UF_SC_CURVE_feature_data_s
Signature
SetAllowedEntityTypes(allowedEntityTypes)
Parameters: allowedEntityTypes ( NXOpen.SectionAllowTypes
) – Allowed entity types.New in version NX7.5.0.
License requirements: gateway (“UG GATEWAY”)
SetInterpart¶
-
Section.
SetInterpart
¶ Set inter-part state of section and make it empty.
This function sets the value of interpart flag on Section. Error will be raised while setting this option on Section in following conditions: (1) Multi-component option is already set on Section.
Signature
SetInterpart(interpart)
Parameters: interpart (bool) – True to set section interpart New in version NX6.0.0.
License requirements: None.
SetMultiComponent¶
-
Section.
SetMultiComponent
¶ Sets the true option on Section for collection from multiple components.
A multi-component Section can have collection from multiple components i.e., multiple parts or multiple instances of same part or both. This method should be used only if such collection is desired. Error will be raised while setting this option on Section in following conditions: (1) Inter-part option is already set on Section.
Signature
SetMultiComponent()
New in version NX9.0.0.
License requirements: None.
SetName¶
-
Section.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetNonFeatureMode¶
-
Section.
SetNonFeatureMode
¶ Sets the true option on Section for collection in non-feature mode.
A Section in non-feature mode does not reference the feature data of the part from which the collection is done. The option should be set on an empty Section only. For a non-empty Section, setting this option will raise error in following conditions: (1) Section is referencing feature data and non-feature mode is set true. (2) Section is not referencing feature data and non-feature mode is set false.
Signature
SetNonFeatureMode()
New in version NX9.0.0.
License requirements: None.
SetStartAndDirection¶
-
Section.
SetStartAndDirection
¶ Sets the start element and the direction of the section.
Signature
SetStartAndDirection(startElement, startPoint, direction)
Parameters: - startElement (
NXOpen.ICurve
) – The element, curve or edge, specifying the starting of the section. If the section is a loop, then the loop is started by start_element and the direction is followed the input direction. If the section is not a loop, then the section can be started by other element, but the direction of the section is defined by the start_element and direction. - startPoint (
NXOpen.Point3d
) – The origin of the vector that defines the direction of the section. This point has to be on the start_element. - direction (
NXOpen.Vector3d
) – The direction of the vector defines the direction of the section.
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
- startElement (
SetStartCurveOfClosedLoop¶
-
Section.
SetStartCurveOfClosedLoop
¶ Set the curve on which the specified point lies as the start curve of a specified single loop of the section.
Signature
SetStartCurveOfClosedLoop(index, pointOnStartCurve)
Parameters: - index (int) – Index of the loop for which the start curve is to be set.
- pointOnStartCurve (
NXOpen.Point3d
) – Any point on a curve that is to be set as the start curve.
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)
SkipSorting¶
-
Section.
SkipSorting
¶ Sets the option to skip sorting the section loops or not.
This method should be used rare scenarios. In normal situation this method should never be used. If sort option is set to true then it should be set to false after required operation is done. If sort option is set to true then section loops are not sorted and output will not be in order.
Signature
SkipSorting(skipSorting)
Parameters: skipSorting (bool) – True to skip sorting of section loops else false New in version NX8.0.0.
License requirements: gateway (“UG GATEWAY”)