SectionDeselectOption Enumeration

NXOpen.Section.DeselectOption is an alias for NXOpen.SectionDeselectOption

class NXOpen.SectionDeselectOption

Bases: object

Defines type of deselect option.

Enum Members

Enum Member Enum Member Description
SectionBetweenIntersection
Potion of the loop between intersections will be deselected this may contain multiple chains
CurveBetweenIntersection Portion of curve between intersection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.