ScalarDimensionalityType Enumeration

NXOpen.Scalar.DimensionalityType is an alias for NXOpen.ScalarDimensionalityType

class NXOpen.ScalarDimensionalityType

Bases: object

Specifies the dimensionality of the scalar.

Enum Members

Enum Member Enum Member Description
NotSet
Length
Area  
Volume
Mass
Angle
Force
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.