VRMLImporterAngularToleranceType Enumeration¶
NXOpen.VRMLImporter.AngularToleranceType is an alias for NXOpen.VRMLImporterAngularToleranceType
-
class
NXOpen.
VRMLImporterAngularToleranceType
¶ Bases:
object
Specifies the angular tolerance.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description Coarse Import with coarse angular tolerance.Medium Import with medium angular tolerance.Fine Import with fine angular tolerance.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-