PolylineCollection Class¶
-
class
NXOpen.
PolylineCollection
¶ Bases:
object
Represents a collection of polylines.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateThroughPoints | Create a polyline from points @return |
FindObject | Finds the Polyline with the given identifier as recorded in a journal. |
Method Detail¶
CreateThroughPoints¶
-
PolylineCollection.
CreateThroughPoints
¶ Create a polyline from points
Signature
CreateThroughPoints(updateOption, points, isClosed)
Parameters: - updateOption (
NXOpen.SmartObjectUpdateOption
) – - points (list of
NXOpen.Point
) – - isClosed (bool) –
Returns: Return type: New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- updateOption (
FindObject¶
-
PolylineCollection.
FindObject
¶ Finds the
Polyline
with the given identifier as recorded in a journal. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the polyline Returns: Return type: NXOpen.Polyline
New in version NX10.0.0.
License requirements: None.